Part Number: TMS320F28027F
Tool/software:
Hello, expert
When we used the F28027F to control the induction motor, we found that in the motor parameter identification process, the value of Rs identified was extremely large (approximately up to 2.3e23). When further conducting the identification, it reached
During the RatedFlux stage, the operation lasted for approximately 5 seconds before an error occurred and the identification process was halted.
May I ask, what could be the possible reasons for this phenomenon?
Motor parameters: 380V, 90W, rated current 0.25A, 50Hz, 2800rpm. These are all the label parameters. There are no more detailed information available.
Looking forward to your reply