TMS320F280049C-Q1: 280049 DCSM module and RAMGS0-3

Part Number: TMS320F280049C-Q1


Tool/software:

If I want to configure DCSM to do JTAG lock[becase 280049 don't have JTAG password mode like 280039], I want to configure all memory to ZONE1, set it to secured, if do that, JTAG is locked.

But I found that RAMGS0-3 can't configure to secured area, so I would like to know what we need to pay attention when using RAMGS0-3? Such as, GS0-3 only can store code, can't store data[In  datasheet, " Data/program reads: Data reads to a secure memory are always blocked unless the program is executing from a memory that belongs to the same zone. Data reads to unsecure memory are always allowed. Table 3-17 shows the levels of security."], so If data is defined in GS0-3, it don't allow these data is read to secure area.

Is my understanding correct?

Best regards.