Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F29H85X-SOM-EVM: Input output Xbar example not working

Part Number: F29H85X-SOM-EVM

Tool/software:

Hi All,

I am trying the following example: C:\ti\f29h85x-sdk_1_01_00_00\examples\driverlib\single_core\xbar\xbar_ex1_input_output.

However, it does not work for me. I even trying feeding a PWM output to the input pin but the output xbar GPIO does not reflect the same state as the input pin.

Am I missing something or is there any other setting that I need to take care.

Thanks,

Mukul