Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Team,
Could you please help with the below question from customer?
Our process has those 2 steps before being able to launch the usb_flash_programmer software.
- Configure the boot mode using a switch SW1 : OFF/OFF = 1/1
- Launch CCS to configure register 0x0D00 to the value 0x0C5A via JTAG, then reset the DSP. The USB device (F28x7x USB Boot Loader) then appears under Windows.
1 - Is there a way to select the correct boot mode without manipulating the switches ?
2 - Is there a way to activate the USB device without configuring register 0x0D00 and resetting the DSP ?
My understanding is customer is using the exact sequence as described in sprujh3 section 4.2.5.
But could the OTP be used to enable USB boot first to program flash, then on the subsequent reboot it is detected that the flash was programmed and CPU1 boots from flash (ie without the step 1) and 2) above).
Thanks in advance,
Anthony