Other Parts Discussed in Thread: TMS320F28335
I am working on familiarizing myself with the flash api for TMS320F28335 and have issues with code allocated to run from ram with the CODE_SECTION pragma causing unexpected interrupts to occur and the system to terminate (as Hwi_unPluggedInterrupt) being called by BIOS6. I have functions outlined as such:
#pragma CODE_SECTION(flashSetup, "FAST_CODE")
int flashSetup(void){...}
#pragma CODE_SECTION(testEraseFlashSector, "FAST_CODE")
void testEraseFlashSector(Uint16 sectorMask, char sectorLetter){..}
#pragma CODE_SECTION(flash_unit_test, "FAST_CODE");
int flash_unit_test(void){...}
Which are copied from flash to ram in my main function before anything is called via:
extern Uint16 FAST_CODE_LOADSTART;
extern Uint16 FAST_CODE_RUNSTART;
extern Uint16 FAST_CODE_LOADSIZE;
memcpy(&FAST_CODE_RUNSTART, &FAST_CODE_LOADSTART, FAST_CODE_LOADSIZE);
With the code section FAST_CODE defined in the CMD file as such:
SECTIONS
{
FAST_CODE:
/*
* Store the code in flash.
*/
LOAD = TFI, PAGE = 0
/*
* Allocate space for all data/code assigned to this section in
* L03 ram or M01 ram. We will have to copy from flash to this
* memory range in code.
*/
RUN = L03SARAM, PAGE = 0
/*
* create a variable FAST_CODE_LOADSTART which sits
* at the start of the FAST_CODE section in flash
*/
LOAD_START(_FAST_CODE_LOADSTART),
/*
* create a var FAST_CODE_LOADSIZE which is the size
* of the FAST_CODE section in flash
*/
LOAD_SIZE(_FAST_CODE_LOADSIZE),
/*
* create a var FAST_CODE_RUNSTART which sits
* at the allocated location in ram for the FAST_CODE code.
*/
RUN_START(_FAST_CODE_RUNSTART)
}
And TFI defined as:
MEMORY
{
PAGE 0: /* Program and Data Memory */
TFI : origin = 0x338000, length = 0x7F80 /* first sector on-chip FLASH */
}
Any idea what I might be doing wrong? I have attached a zip of my project: