Part Number: F29H85X-SOM-EVM
Tool/software:
When I load MCU_Core1 program, I get this error message:
C29xx_CPU1: Error during Flash Programming. Program command was not issued since address provided for Flash program operation is invalid. Address provided is 0xFFFFFFFF
C29xx_CPU1: An attempt was made to program to an address not within this Bank Mode.
C29xx_CPU1: Please ensure that you have programmed the correct Bank Mode prior to flash programming.
C29xx_CPU1: File Loader: Memory write failed: Unknown error
C29xx_CPU1: GEL: File: C:\Users\Desktop\mcu-main\MCU_Core1\FLASH\MCU_Core1.out: Load failed.
File: C:\Users\Desktop\main\MCU_Core1\FLASH\MCU_Core1.out: Load failed.
What could be the reason?