Part Number: TMS320F28P650DH
Other Parts Discussed in Thread: UNIFLASH
Tool/software:
Hi Experts,
I have trouble using UniFlash CLI to program CPU2. Below are the steps I took.
1. Configure the uniflash GUI correctly, ensure I can program both CPU1 and CPU2 in the GUI.
2, Click generate package.
3. Unzip the generated zip file.
4. Execute dslite-C28xx_CPU1.bat and dslite-C28xx_CPU2.bat respectively.
The execution of dslite-C28xx_CPU1.bat is successful, however the execution of dslite-C28xx_CPU2.bat fails, the error message is
"Error erasing Bank 2 FMSTAT (STATCMD on some devices) value = 65 (decimal)"
Where Bank2 is the first bank I use for CPU2 program.
My guess is the clock configuration that cuase this issue, which is informed in the GUI as below.

Nevertheless, I didn't find any way to configure the clock in the CPU2 standalone command.
How to program CPU2 using CLI?
Regards,
Hang