Part Number: TMS320F280039
Other Parts Discussed in Thread: LM2901,
Tool/software:
customer report the internal pull down resistance value looks much difference in low temperature, they do the test as below, please help review if it make sense?
Below is their circuit, LM2901 output to F280039 IO (signal mark as 12VOVP_GLBLE) through diode DA125, with external cap (1nF) in the IO which enable internal pull down.
LM2901 output high at beginning so that CAP will be charged, then LM2901 output low so that CAP should discharge through IO internal pull down resistor.
1, In 25c normal temperature, read the IO status from high to low <1 second
2, In -40c low temperature, read the IO status from high to low >15 second
3, In -40c low temperature, add external 20K pull down resistor in the IO, read IO status from high to low <1 second