Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: ADC converter operation

Part Number: TMS320F28388D

Tool/software:

The part in question (TMS320F28388D) has 4 ADC converter peripherals.  Almost all of the pins are mapped to a particular converter, for example ADCINA0, ADCINB1, ADCIND4 etc.  However there are 2 pins T4 and U4 that have no ADC block associated with them.  For example T4 is labelled ADCIN14 and U4 is labelled ADCIN15.  If I want to provide analog signals to be converted on those 2 pins which of the 4 converter peripherals (A, B, C or D) do I use?