This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P550SG: Any QFN package with 64 pins

Part Number: TMS320F28P550SG

Hi,

Due to are constraints, I'd like to use a QFN package and 56 package MCUs are just a little too small. Is there any MCU series from C2000 which is 64 pins and QFN? Well any other package variation would also help. The one I'm currently considering is TQFP80 and it's pretty large.

Thanks and regards