Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Hello.
I'm studying for development.
I would like to inquire about the problems that arise in the process of developing CAN communication in a bit field method.
The development environment is as follows.
MCU : f28388d
CCS version: 12.8.1.00005
CCS Compiler Version: TI v22.6.3.LTS
c2000Ware version: 6.00.00
- Predefined: [CPU1], [USE_20MHZ_XTAL]
I'm only using CPU1, and I don't use CLA as below. The compiler version is also higher than 16, but "f2838x_can.h" is not enabled.
- I tried turning CLA support on or off, but it didn't work.
- I tried changing the compilation version to the previous version, but it didn't work.
I need help with what the problem is.
Thank you.