Other Parts Discussed in Thread: UCC28070EVM
Hi,
I have one problem with the graphs at CCSv5.
When I open the graphs with Tools -> Graph -> single or Dual Time, and then I put there all Datas like in the "CCS User Guide for Power Factor Correction on UCC28070EVM Using C2000 Piccolo-A", and then I click on Ok. Then it shows me only a line on the botton for the graph field. How can I put the the line with I want? I have still used DBUFF1 / 2 / 3 and 4. If I put there e.g. "PFCDuty" or "Gui_VpfcSet" I get no information.
If I open the graph with a rightclick on the Expressions and then on graph, then I get the graph of the Expression. But only I the slow version, with a value with I have put Customize Continuous Refresh Interval- menu.
How is possible to get faster informations? It doesn't care with the rightclick possible or with the Tools - Graph- Dual Time possible? I want to get a graph like in the "CCS User Guide for Power Factor Correction on UCC28070EVM Using C2000 Piccolo-A" shown on page 21 or 31.
Thank you,
Friedbert Maier