Hello,
We have been reading the application note regarding bissc implementation on devices like f28p255 wqith CLB. I would like to confirm the hardware requirements as we are passing from a 64 pin mcu to 56 pin mcu with only 2 CLBs, therfore, for that application, which are the pins, and peripheral reservations in total.
- 2 pins in total? One corresponding to epwm and the other one corresponding to SPIMOSI?
- EPWM4 or it can be anyone
- 1 SPI?
Is there any place where we can obtain the original source code?
Regards,
David