This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: Missing implementation of EPWM_setSyncOutPulseMode in F2838x version of driverlib

Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE

Hi Experts,

the F2838x veriosn of the driverlib has this entry:

./driverlib/f2838x/driverlib/hrpwm.h:229:#define HRPWM_setSyncOutPulseMode                EPWM_setSyncOutPulseMode

However, unlike F28379xD, there is no implementation of EPWM_setSyncOutPulseMode().

Here is the grep results:

~/opt/ti/c2000/C2000Ware_6_00_00_00
$ grep EPWM_setSyncOutPulseMode --include=*.h -nIr .
./driverlib/f280013x/driverlib/hrpwm.h:227:#define HRPWM_setSyncOutPulseMode                EPWM_setSyncOutPulseMode
./driverlib/f280015x/driverlib/hrpwm.h:227:#define HRPWM_setSyncOutPulseMode                EPWM_setSyncOutPulseMode
./driverlib/f28002x/driverlib/hrpwm.h:227:#define HRPWM_setSyncOutPulseMode                EPWM_setSyncOutPulseMode
./driverlib/f28003x/driverlib/hrpwm.h:227:#define HRPWM_setSyncOutPulseMode                EPWM_setSyncOutPulseMode
./driverlib/f28004x/driverlib/epwm.h:140://! Values that can be passed to EPWM_setSyncOutPulseMode() as the \e mode
./driverlib/f28004x/driverlib/epwm.h:1694:EPWM_setSyncOutPulseMode(uint32_t base, EPWM_SyncOutPulseMode mode)
./driverlib/f28004x/driverlib/hrpwm.h:227:#define HRPWM_setSyncOutPulseMode                EPWM_setSyncOutPulseMode
./driverlib/f2807x/driverlib/epwm.h:143://! Values that can be passed to EPWM_setSyncOutPulseMode() as the \e mode
./driverlib/f2807x/driverlib/epwm.h:1691:EPWM_setSyncOutPulseMode(uint32_t base, EPWM_SyncOutPulseMode mode)
./driverlib/f2807x/driverlib/hrpwm.h:229:#define HRPWM_setSyncOutPulseMode                EPWM_setSyncOutPulseMode
./driverlib/f2837xd/driverlib/epwm.h:143://! Values that can be passed to EPWM_setSyncOutPulseMode() as the \e mode
./driverlib/f2837xd/driverlib/epwm.h:1691:EPWM_setSyncOutPulseMode(uint32_t base, EPWM_SyncOutPulseMode mode)
./driverlib/f2837xd/driverlib/hrpwm.h:229:#define HRPWM_setSyncOutPulseMode                EPWM_setSyncOutPulseMode
./driverlib/f2837xs/driverlib/epwm.h:143://! Values that can be passed to EPWM_setSyncOutPulseMode() as the \e mode
./driverlib/f2837xs/driverlib/epwm.h:1691:EPWM_setSyncOutPulseMode(uint32_t base, EPWM_SyncOutPulseMode mode)
./driverlib/f2837xs/driverlib/hrpwm.h:229:#define HRPWM_setSyncOutPulseMode                EPWM_setSyncOutPulseMode
./driverlib/f2838x/driverlib/hrpwm.h:229:#define HRPWM_setSyncOutPulseMode                EPWM_setSyncOutPulseMode
./driverlib/f28p55x/driverlib/hrpwm.h:229:#define HRPWM_setSyncOutPulseMode                EPWM_setSyncOutPulseMode
./driverlib/f28p65x/driverlib/hrpwm.h:232:#define HRPWM_setSyncOutPulseMode                EPWM_setSyncOutPulseMode
./libraries/boot_rom/f28002x/rev0/rom_sources/F28002x_ROM/driverlib/hrpwm.h:232:#define HRPWM_setSyncOutPulseMode                EPWM_setSyncOutPulseMode
./libraries/boot_rom/f28004x/rev0/rom_sources/F28004x_ROM/driverlib/epwm.h:131:// Values that can be passed to EPWM_setSyncOutPulseMode() as the mode
./libraries/boot_rom/f28004x/rev0/rom_sources/F28004x_ROM/driverlib/epwm.h:1311:static inline void EPWM_setSyncOutPulseMode(uint32_t base,
./libraries/boot_rom/f28004x/rev0/rom_sources/F28004x_ROM/driverlib/hrpwm.h:218:#define HRPWM_setSyncOutPulseMode                EPWM_setSyncOutPulseMode
./libraries/boot_rom/f28004x/revA/rom_sources/F28004x_ROM/driverlib/epwm.h:131:// Values that can be passed to EPWM_setSyncOutPulseMode() as the mode
./libraries/boot_rom/f28004x/revA/rom_sources/F28004x_ROM/driverlib/epwm.h:1311:static inline void EPWM_setSyncOutPulseMode(uint32_t base,
./libraries/boot_rom/f28004x/revA/rom_sources/F28004x_ROM/driverlib/hrpwm.h:218:#define HRPWM_setSyncOutPulseMode                EPWM_setSyncOutPulseMode
./libraries/boot_rom/f28004x/revB/rom_sources/F28004x_ROM/driverlib/epwm.h:131:// Values that can be passed to EPWM_setSyncOutPulseMode() as the mode
./libraries/boot_rom/f28004x/revB/rom_sources/F28004x_ROM/driverlib/epwm.h:1311:static inline void EPWM_setSyncOutPulseMode(uint32_t base,
./libraries/boot_rom/f28004x/revB/rom_sources/F28004x_ROM/driverlib/hrpwm.h:218:#define HRPWM_setSyncOutPulseMode                EPWM_setSyncOutPulseMode
./libraries/boot_rom/f2838x/rev0/rom_sources/cpu1/F2838x_ROM/driverlib/hrpwm.h:232:#define HRPWM_setSyncOutPulseMode                EPWM_setSyncOutPulseMode
./libraries/boot_rom/f2838x/rev0/rom_sources/cpu2/F2838x_ROM/driverlib/hrpwm.h:232:#define HRPWM_setSyncOutPulseMode                EPWM_setSyncOutPulseMode
./libraries/boot_rom/f2838x/revA/rom_sources/cpu1/F2838x_ROM/driverlib/hrpwm.h:232:#define HRPWM_setSyncOutPulseMode                EPWM_setSyncOutPulseMode
./libraries/boot_rom/f2838x/revA/rom_sources/cpu2/F2838x_ROM/driverlib/hrpwm.h:232:#define HRPWM_setSyncOutPulseMode                EPWM_setSyncOutPulseMode

Regards,

Marvin

  • Hi Marvin

    Yes, you are correct. The EPWM_setSyncOutPulseMode is not present for F2838x since SYNCOSEL bit (In TBCTL register) was removed. Instead, they have added 

    SYNCOUTEN register which has the same functionality and there is a separate API (EPWM_enableSyncOutPulseSource) in the driverlib to configure SYNCOUTEN.
    So, the HRPWM_setSyncOutPulseMode should be mapped to EPWM_enableSyncOutPulseSource API as below:
    #define HRPWM_setSyncOutPulseMode                EPWM_enableSyncOutPulseSource
    Regards,

    Meghavi