Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280034: F280034 Serial_Flash_programmer Freezing

Part Number: TMS320F280034
Other Parts Discussed in Thread: C2000WARE

After SCI Boot, I completed sending Kernel through Serial flash programmer, but it stopped after completion of sending(CMD Command : serial_flash_programmer -d f28003x -k f28003x_flash_kernel.txt -a pm_control.txt -p COM14)

After the transmission is completed, it is stopped as shown in the picture below 

image.png

f28003x_flash_kernel.txt 

  • Hello,

    Can you connect to the device in CCS and load the symbols for the kernel to see the current state? Could you also confirm that the correct SCI TX/RX GPIOs are being used by the flash kernel?

    Best,

    Matt

  • The GPIO setting for SCI booting is set up properly, and after SCI booting, kernel transmission has completed, and as shown in the above picture, kernel has stopped. I didn't understand at all about connecting to CCS using Kernel Symbol. Please explain in detail.

  • Hello,

    Once the kernel is loaded and stuck in execution, please do the following:

    1. In CCS, go to "View" > "Target Configurations"
    2. The Target Configuration window will pop up. Right click the target configuration from your project (or you can import one from C2000Ware) and select "Launch Selected Configuration"
    3. The Debug window will pop up. Right click CPU1 and select "Connect to target"
    4. Once you've connected, navigate to "Load" > "Load Symbols" in the taskbar.
    5. Select the kernel .out file to load the kernel's symbols. The current state of the device in the kernel will now display in CCS and you can now debug the issue.

    Best,

    Matt

  • After SCI booting, insert Kernel through SCI after completing the transmission as in the CMD window above,and download the symbol using the method you told me  and it comes out like the attached picture

    Unable to load symbol.What should I check first?

  • Hello,

    It looks like the device isn't executing the kernel (the program counter is in the boot ROM), which is why loading the symbols failed to reveal anything. 

    I also successfully executed the SCI boot flow on my F28003x LaunchPad, can you please try using this flash kernel?

    
    AA 08 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 02 00 
    00 00 00 00 40 00 69 9E 
    34 01 00 00 28 01 04 FE 43 7C 42 1E 40 76 8C A1 00 52 06 60 00 8F 90 A8 
    3F 02 40 76 EB A2 48 06 40 76 9C A1 00 52 06 60 00 8F 90 A8 40 02 40 76 
    EB A2 43 92 0F 52 06 69 00 8F 90 A8 41 02 40 76 EB A2 42 06 00 D4 03 D5 
    40 76 71 01 01 D4 03 D5 42 06 40 76 71 01 02 D4 03 D5 42 06 40 76 71 01 
    01 D4 42 06 40 76 C1 01 42 06 40 76 DE 01 42 06 40 76 F6 01 43 5C 42 06 
    40 76 9D 01 42 06 40 76 0E 02 42 06 40 76 25 02 48 06 40 76 3C 02 07 F6 
    00 77 69 FF 84 FE 06 00 04 FE 44 7D 43 7C 42 1E 40 76 8C A1 00 52 07 60 
    20 FF 31 01 00 8F 42 A8 40 76 EB A2 22 76 44 27 AA 2B 03 56 43 01 A9 16 
    3B 56 5A FF 03 56 43 01 A9 2D 03 9A 66 FF 5E FF A9 88 20 02 42 07 A9 8A 
    C4 06 A6 89 AB CA AA CB A7 1E 20 02 42 07 A9 8A C4 C3 1A 76 84 FE 06 00 
    04 FE 43 7C 42 1E 40 76 8C A1 00 52 07 60 20 FF 01 01 00 8F 42 A8 40 76 
    EB A2 43 92 0F 52 07 69 20 FF 06 01 00 8F 42 A8 40 76 EB A2 22 76 42 8A 
    01 29 03 56 43 08 C4 A3 AB 18 FF F0 AA CB AB CA C4 1E 1A 76 84 FE 06 00 
    04 FE 43 7C 42 1E 40 76 8C A1 00 52 07 60 20 FF 57 01 00 8F 42 A8 40 76 
    EB A2 22 76 24 02 42 07 A9 8A C4 06 A9 18 FE FF 43 AF A6 1E 24 02 42 07 
    A9 8A C4 C2 1A 76 84 FE 06 00 02 FE 42 1E 40 76 8C A1 00 52 07 60 20 FF 
    D0 01 00 8F 42 A8 40 76 EB A2 22 76 20 FF 80 01 42 07 A9 8A C4 06 A9 18 
    FD FF C4 1E 1A 76 82 FE 06 00 02 FE 42 1E 40 76 8C A1 00 52 07 60 20 FF 
    94 01 00 8F 42 A8 40 76 EB A2 22 76 20 FF 80 01 42 07 A9 8A C4 06 A9 18 
    FE FF C4 1E 1A 76 82 FE 06 00 02 FE 42 1E 40 76 8C A1 00 52 07 60 20 FF 
    B2 01 00 8F 42 A8 40 76 EB A2 22 76 20 FF 80 01 42 07 A9 8A 02 02 C4 98 
    CC 99 1A 76 82 FE 06 00 02 FE 42 1E 40 76 8C A1 00 52 07 60 20 FF 76 01 
    00 8F 42 A8 40 76 EB A2 22 76 20 FF 80 01 42 07 A9 8A 01 02 C4 98 CC 99 
    1A 76 82 FE 06 00 02 FE 42 1E 40 76 9C A1 00 52 07 60 20 FF EE 01 00 8F 
    42 A8 40 76 EB A2 22 76 42 8A C4 06 A9 18 F0 FF 0A 50 C4 1E 1A 76 82 FE 
    06 00 02 FE 41 96 25 76 69 FF 82 FE 06 00 01 19 C3 56 FF FF 06 00 
    18 00 00 00 5C 02 01 00 01 00 00 00 0F 00 1E 00 F0 FF 65 A2 00 00 71 9C 
    00 00 BE A2 00 00 00 00 00 00 12 00 00 00 5C 02 00 00 00 A8 00 00 68 02 
    00 00 30 A8 00 00 
    C6 02 00 00 42 A8 2F 00 68 00 6F 00 6D 00 65 00 2F 00 75 00 62 00 6E 00 
    75 00 73 00 65 00 72 00 2F 00 74 00 69 00 2F 00 72 00 65 00 70 00 6F 00 
    73 00 2F 00 63 00 32 00 30 00 30 00 30 00 77 00 61 00 72 00 65 00 5F 00 
    72 00 65 00 6C 00 65 00 61 00 73 00 65 00 2F 00 64 00 72 00 69 00 76 00 
    65 00 72 00 6C 00 69 00 62 00 2F 00 66 00 32 00 38 00 30 00 30 00 33 00 
    78 00 2F 00 64 00 72 00 69 00 76 00 65 00 72 00 6C 00 69 00 62 00 2F 00 
    66 00 6C 00 61 00 73 00 68 00 2E 00 68 00 00 00 00 00 2F 00 68 00 6F 00 
    6D 00 65 00 2F 00 75 00 62 00 6E 00 75 00 73 00 65 00 72 00 2F 00 74 00 
    69 00 2F 00 72 00 65 00 70 00 6F 00 73 00 2F 00 63 00 32 00 30 00 30 00 
    30 00 77 00 61 00 72 00 65 00 5F 00 72 00 65 00 6C 00 65 00 61 00 73 00 
    65 00 2F 00 64 00 72 00 69 00 76 00 65 00 72 00 6C 00 69 00 62 00 2F 00 
    66 00 32 00 38 00 30 00 30 00 33 00 78 00 2F 00 64 00 72 00 69 00 76 00 
    65 00 72 00 6C 00 69 00 62 00 2F 00 66 00 6C 00 61 00 73 00 68 00 2E 00 
    63 00 00 00 00 00 2F 00 68 00 6F 00 6D 00 65 00 2F 00 75 00 62 00 6E 00 
    75 00 73 00 65 00 72 00 2F 00 74 00 69 00 2F 00 72 00 65 00 70 00 6F 00 
    73 00 2F 00 63 00 32 00 30 00 30 00 30 00 77 00 61 00 72 00 65 00 5F 00 
    72 00 65 00 6C 00 65 00 61 00 73 00 65 00 2F 00 64 00 72 00 69 00 76 00 
    65 00 72 00 6C 00 69 00 62 00 2F 00 66 00 32 00 38 00 30 00 30 00 33 00 
    78 00 2F 00 64 00 72 00 69 00 76 00 65 00 72 00 6C 00 69 00 62 00 2F 00 
    64 00 63 00 63 00 2E 00 68 00 00 00 00 00 2F 00 68 00 6F 00 6D 00 65 00 
    2F 00 75 00 62 00 6E 00 75 00 73 00 65 00 72 00 2F 00 74 00 69 00 2F 00 
    72 00 65 00 70 00 6F 00 73 00 2F 00 63 00 32 00 30 00 30 00 30 00 77 00 
    61 00 72 00 65 00 5F 00 72 00 65 00 6C 00 65 00 61 00 73 00 65 00 2F 00 
    64 00 72 00 69 00 76 00 65 00 72 00 6C 00 69 00 62 00 2F 00 66 00 32 00 
    38 00 30 00 30 00 33 00 78 00 2F 00 64 00 72 00 69 00 76 00 65 00 72 00 
    6C 00 69 00 62 00 2F 00 73 00 79 00 73 00 63 00 74 00 6C 00 2E 00 63 00 
    00 00 2F 00 68 00 6F 00 6D 00 65 00 2F 00 75 00 62 00 6E 00 75 00 73 00 
    65 00 72 00 2F 00 74 00 69 00 2F 00 72 00 65 00 70 00 6F 00 73 00 2F 00 
    63 00 32 00 30 00 30 00 30 00 77 00 61 00 72 00 65 00 5F 00 72 00 65 00 
    6C 00 65 00 61 00 73 00 65 00 2F 00 64 00 72 00 69 00 76 00 65 00 72 00 
    6C 00 69 00 62 00 2F 00 66 00 32 00 38 00 30 00 30 00 33 00 78 00 2F 00 
    64 00 72 00 69 00 76 00 65 00 72 00 6C 00 69 00 62 00 2F 00 78 00 62 00 
    61 00 72 00 2E 00 68 00 00 00 2F 00 68 00 6F 00 6D 00 65 00 2F 00 75 00 
    62 00 6E 00 75 00 73 00 65 00 72 00 2F 00 74 00 69 00 2F 00 72 00 65 00 
    70 00 6F 00 73 00 2F 00 63 00 32 00 30 00 30 00 30 00 77 00 61 00 72 00 
    65 00 5F 00 72 00 65 00 6C 00 65 00 61 00 73 00 65 00 2F 00 64 00 72 00 
    69 00 76 00 65 00 72 00 6C 00 69 00 62 00 2F 00 66 00 32 00 38 00 30 00 
    30 00 33 00 78 00 2F 00 64 00 72 00 69 00 76 00 65 00 72 00 6C 00 69 00 
    62 00 2F 00 67 00 70 00 69 00 6F 00 2E 00 63 00 00 00 2F 00 68 00 6F 00 
    6D 00 65 00 2F 00 75 00 62 00 6E 00 75 00 73 00 65 00 72 00 2F 00 74 00 
    69 00 2F 00 72 00 65 00 70 00 6F 00 73 00 2F 00 63 00 32 00 30 00 30 00 
    30 00 77 00 61 00 72 00 65 00 5F 00 72 00 65 00 6C 00 65 00 61 00 73 00 
    65 00 2F 00 64 00 72 00 69 00 76 00 65 00 72 00 6C 00 69 00 62 00 2F 00 
    66 00 32 00 38 00 30 00 30 00 33 00 78 00 2F 00 64 00 72 00 69 00 76 00 
    65 00 72 00 6C 00 69 00 62 00 2F 00 73 00 63 00 69 00 2E 00 68 00 00 00 
    00 00 2F 00 68 00 6F 00 6D 00 65 00 2F 00 75 00 62 00 6E 00 75 00 73 00 
    65 00 72 00 2F 00 74 00 69 00 2F 00 72 00 65 00 70 00 6F 00 73 00 2F 00 
    63 00 32 00 30 00 30 00 30 00 77 00 61 00 72 00 65 00 5F 00 72 00 65 00 
    6C 00 65 00 61 00 73 00 65 00 2F 00 64 00 72 00 69 00 76 00 65 00 72 00 
    6C 00 69 00 62 00 2F 00 66 00 32 00 38 00 30 00 30 00 33 00 78 00 2F 00 
    64 00 72 00 69 00 76 00 65 00 72 00 6C 00 69 00 62 00 2F 00 73 00 63 00 
    69 00 2E 00 63 00 00 00 00 00 00 00 08 00 00 10 08 00 00 20 08 00 00 30 
    08 00 00 40 08 00 00 50 08 00 00 60 08 00 00 70 08 00 00 80 08 00 00 90 
    08 00 00 A0 08 00 00 B0 08 00 00 C0 08 00 00 D0 08 00 00 E0 08 00 00 F0 
    08 00 00 00 09 00 00 10 09 00 00 20 09 00 00 30 09 00 00 40 09 00 00 50 
    09 00 00 60 09 00 00 70 09 00 00 80 09 00 00 90 09 00 00 A0 09 00 00 B0 
    09 00 00 C0 09 00 00 D0 09 00 00 E0 09 00 00 F0 09 00 00 00 0A 00 00 10 
    0A 00 00 20 0A 00 00 30 0A 00 00 40 0A 00 00 50 0A 00 00 60 0A 00 00 70 
    0A 00 00 80 0A 00 00 90 0A 00 00 A0 0A 00 00 B0 0A 00 00 C0 0A 00 00 D0 
    0A 00 00 E0 0A 00 00 F0 0A 00 
    FF 07 00 00 00 80 02 FE 42 1E 08 8F 00 00 A9 A8 42 0F 10 66 08 8F 00 10 
    A9 A8 42 0F 0B 69 1F 76 A0 02 00 92 07 60 BF 56 00 01 08 8F 00 00 EF FF 
    AC 03 08 8F 00 10 A9 A8 42 0F 10 66 08 8F 00 20 A9 A8 42 0F 0B 69 1F 76 
    A0 02 01 92 07 60 BF 56 01 01 08 8F 00 10 EF FF 98 03 08 8F 00 20 A9 A8 
    42 0F 10 66 08 8F 00 30 A9 A8 42 0F 0B 69 1F 76 A0 02 02 92 07 60 BF 56 
    02 01 08 8F 00 20 EF FF 84 03 08 8F 00 30 A9 A8 42 0F 10 66 08 8F 00 40 
    A9 A8 42 0F 0B 69 1F 76 A0 02 03 92 07 60 BF 56 03 01 08 8F 00 30 EF FF 
    70 03 08 8F 00 40 A9 A8 42 0F 10 66 08 8F 00 50 A9 A8 42 0F 0B 69 1F 76 
    A0 02 04 92 07 60 BF 56 04 01 08 8F 00 40 EF FF 5C 03 08 8F 00 50 A9 A8 
    42 0F 10 66 08 8F 00 60 A9 A8 42 0F 0B 69 1F 76 A0 02 05 92 07 60 BF 56 
    05 01 08 8F 00 50 EF FF 48 03 08 8F 00 60 A9 A8 42 0F 10 66 08 8F 00 70 
    A9 A8 42 0F 0B 69 1F 76 A0 02 06 92 07 60 BF 56 06 01 08 8F 00 60 EF FF 
    34 03 08 8F 00 70 A9 A8 42 0F 10 66 08 8F 00 80 A9 A8 42 0F 0B 69 1F 76 
    A0 02 07 92 07 60 BF 56 07 01 08 8F 00 70 EF FF 20 03 08 8F 00 80 A9 A8 
    42 0F 10 66 08 8F 00 90 A9 A8 42 0F 0B 69 1F 76 A0 02 08 92 07 60 BF 56 
    08 01 08 8F 00 80 EF FF 0C 03 08 8F 00 90 A9 A8 42 0F 10 66 08 8F 00 A0 
    A9 A8 42 0F 0B 69 1F 76 A0 02 09 92 07 60 BF 56 09 01 08 8F 00 90 EF FF 
    F8 02 08 8F 00 A0 A9 A8 42 0F 10 66 08 8F 00 B0 A9 A8 42 0F 0B 69 1F 76 
    A0 02 0A 92 07 60 BF 56 0A 01 08 8F 00 A0 EF FF E4 02 08 8F 00 B0 A9 A8 
    42 0F 10 66 08 8F 00 C0 A9 A8 42 0F 0B 69 1F 76 A0 02 0B 92 07 60 BF 56 
    0B 01 08 8F 00 B0 EF FF D0 02 08 8F 00 C0 A9 A8 42 0F 10 66 08 8F 00 D0 
    A9 A8 42 0F 0B 69 1F 76 A0 02 0C 92 07 60 BF 56 0C 01 08 8F 00 C0 EF FF 
    BC 02 08 8F 00 D0 A9 A8 42 0F 10 66 08 8F 00 E0 A9 A8 42 0F 0B 69 1F 76 
    A0 02 0D 92 07 60 BF 56 0D 01 08 8F 00 D0 EF FF A8 02 08 8F 00 E0 A9 A8 
    42 0F 10 66 08 8F 00 F0 A9 A8 42 0F 0B 69 1F 76 A0 02 0E 92 07 60 BF 56 
    0E 01 08 8F 00 E0 EF FF 94 02 08 8F 00 F0 A9 A8 42 0F 10 66 08 8F FF FF 
    A9 A8 42 0F 0B 68 1F 76 A0 02 0F 92 07 60 BF 56 0F 01 08 8F 00 F0 EF FF 
    80 02 09 8F 00 00 A9 A8 42 0F 10 66 09 8F 00 10 A9 A8 42 0F 0B 69 1F 76 
    A0 02 10 92 07 60 BF 56 10 01 09 8F 00 00 EF FF 6C 02 09 8F 00 10 A9 A8 
    42 0F 10 66 09 8F 00 20 A9 A8 42 0F 0B 69 1F 76 A0 02 11 92 07 60 BF 56 
    11 01 09 8F 00 10 EF FF 58 02 09 8F 00 20 A9 A8 42 0F 10 66 09 8F 00 30 
    A9 A8 42 0F 0B 69 1F 76 A0 02 12 92 07 60 BF 56 12 01 09 8F 00 20 EF FF 
    44 02 09 8F 00 30 A9 A8 42 0F 10 66 09 8F 00 40 A9 A8 42 0F 0B 69 1F 76 
    A0 02 13 92 07 60 BF 56 13 01 09 8F 00 30 EF FF 30 02 09 8F 00 40 A9 A8 
    42 0F 10 66 09 8F 00 50 A9 A8 42 0F 0B 69 1F 76 A0 02 14 92 07 60 BF 56 
    14 01 09 8F 00 40 EF FF 1C 02 09 8F 00 50 A9 A8 42 0F 10 66 09 8F 00 60 
    A9 A8 42 0F 0B 69 1F 76 A0 02 15 92 07 60 BF 56 15 01 09 8F 00 50 EF FF 
    08 02 09 8F 00 60 A9 A8 42 0F 10 66 09 8F 00 70 A9 A8 42 0F 0B 69 1F 76 
    A0 02 16 92 07 60 BF 56 16 01 09 8F 00 60 EF FF F4 01 09 8F 00 70 A9 A8 
    42 0F 10 66 09 8F 00 80 A9 A8 42 0F 0B 69 1F 76 A0 02 17 92 07 60 BF 56 
    17 01 09 8F 00 70 EF FF E0 01 09 8F 00 80 A9 A8 42 0F 10 66 09 8F 00 90 
    A9 A8 42 0F 0B 69 1F 76 A0 02 18 92 07 60 BF 56 18 01 09 8F 00 80 EF FF 
    CC 01 09 8F 00 90 A9 A8 42 0F 10 66 09 8F 00 A0 A9 A8 42 0F 0B 69 1F 76 
    A0 02 19 92 07 60 BF 56 19 01 09 8F 00 90 EF FF B8 01 09 8F 00 A0 A9 A8 
    42 0F 10 66 09 8F 00 B0 A9 A8 42 0F 0B 69 1F 76 A0 02 1A 92 07 60 BF 56 
    1A 01 09 8F 00 A0 EF FF A4 01 09 8F 00 B0 A9 A8 42 0F 10 66 09 8F 00 C0 
    A9 A8 42 0F 0B 69 1F 76 A0 02 1B 92 07 60 BF 56 1B 01 09 8F 00 B0 EF FF 
    90 01 09 8F 00 C0 A9 A8 42 0F 10 66 09 8F 00 D0 A9 A8 42 0F 0B 69 1F 76 
    A0 02 1C 92 07 60 BF 56 1C 01 09 8F 00 C0 EF FF 7C 01 09 8F 00 D0 A9 A8 
    42 0F 10 66 09 8F 00 E0 A9 A8 42 0F 0B 69 1F 76 A0 02 1D 92 07 60 BF 56 
    1D 01 09 8F 00 D0 EF FF 68 01 09 8F 00 E0 A9 A8 42 0F 10 66 09 8F 00 F0 
    A9 A8 42 0F 0B 69 1F 76 A0 02 1E 92 07 60 BF 56 1E 01 09 8F 00 E0 EF FF 
    54 01 09 8F 00 F0 A9 A8 42 0F 10 66 0A 8F 00 10 A9 A8 42 0F 0B 68 1F 76 
    A0 02 1F 92 07 60 BF 56 1F 01 09 8F 00 F0 EF FF 40 01 0A 8F 00 00 A9 A8 
    42 0F 10 66 0A 8F 00 10 A9 A8 42 0F 0B 69 1F 76 A0 02 20 92 07 60 BF 56 
    20 01 0A 8F 00 00 EF FF 2C 01 0A 8F 00 10 A9 A8 42 0F 10 66 0A 8F 00 20 
    A9 A8 42 0F 0B 69 1F 76 A0 02 21 92 07 60 BF 56 21 01 0A 8F 00 10 EF FF 
    18 01 0A 8F 00 20 A9 A8 42 0F 10 66 0A 8F 00 30 A9 A8 42 0F 0B 69 1F 76 
    A0 02 22 92 07 60 BF 56 22 01 0A 8F 00 20 EF FF 04 01 0A 8F 00 30 A9 A8 
    42 0F 10 66 0A 8F 00 40 A9 A8 42 0F 0B 69 1F 76 A0 02 23 92 07 60 BF 56 
    23 01 0A 8F 00 30 EF FF F0 00 0A 8F 00 40 A9 A8 42 0F 10 66 0A 8F 00 50 
    A9 A8 42 0F 0B 69 1F 76 A0 02 24 92 07 60 BF 56 24 01 0A 8F 00 40 EF FF 
    DC 00 0A 8F 00 50 A9 A8 42 0F 10 66 0A 8F 00 60 A9 A8 42 0F 0B 69 1F 76 
    A0 02 25 92 07 60 BF 56 25 01 0A 8F 00 50 EF FF C8 00 0A 8F 00 60 A9 A8 
    42 0F 10 66 0A 8F 00 70 A9 A8 42 0F 0B 69 1F 76 A0 02 26 92 07 60 BF 56 
    26 01 0A 8F 00 60 EF FF B4 00 0A 8F 00 70 A9 A8 42 0F 10 66 0A 8F 00 80 
    A9 A8 42 0F 0B 69 1F 76 A0 02 27 92 07 60 BF 56 27 01 0A 8F 00 70 EF FF 
    A0 00 0A 8F 00 80 A9 A8 42 0F 10 66 0A 8F 00 90 A9 A8 42 0F 0B 69 1F 76 
    A0 02 28 92 07 60 BF 56 28 01 0A 8F 00 80 EF FF 8C 00 0A 8F 00 90 A9 A8 
    42 0F 0F 66 0A 8F 00 A0 A9 A8 42 0F 0A 69 1F 76 A0 02 29 92 06 60 BF 56 
    29 01 0A 8F 00 90 78 6F 0A 8F 00 A0 A9 A8 42 0F 0F 66 0A 8F 00 B0 A9 A8 
    42 0F 0A 69 1F 76 A0 02 2A 92 06 60 BF 56 2A 01 0A 8F 00 A0 65 6F 0A 8F 
    00 B0 A9 A8 42 0F 0F 66 0A 8F 00 C0 A9 A8 42 0F 0A 69 1F 76 A0 02 2B 92 
    06 60 BF 56 2B 01 0A 8F 00 B0 52 6F 0A 8F 00 C0 A9 A8 42 0F 0F 66 0A 8F 
    00 D0 A9 A8 42 0F 0A 69 1F 76 A0 02 2C 92 06 60 BF 56 2C 01 0A 8F 00 C0 
    3F 6F 0A 8F 00 D0 A9 A8 42 0F 0F 66 0A 8F 00 E0 A9 A8 42 0F 0A 69 1F 76 
    A0 02 2D 92 06 60 BF 56 2D 01 0A 8F 00 D0 2C 6F 0A 8F 00 E0 A9 A8 42 0F 
    0F 66 0A 8F 00 F0 A9 A8 42 0F 0A 69 1F 76 A0 02 2E 92 06 60 BF 56 2E 01 
    0A 8F 00 E0 19 6F 0A 8F 00 F0 A9 A8 42 0F 0F 66 0A 8F FF FF A9 A8 42 0F 
    0A 68 1F 76 A0 02 2F 92 06 60 BF 56 2F 01 0A 8F 00 F0 06 6F A9 28 EF BE 
    A8 28 AD DE A9 8A 82 FE A9 A8 06 00 BD AA AD 5A 84 DA 4C FE FA 96 00 02 
    10 D0 92 1E 0E D0 92 1E 0C D0 92 1E F2 2B 0A D0 92 1E 01 29 07 8F A8 00 
    03 56 FA 0A 01 56 A4 00 08 D0 92 A8 08 D0 92 06 7E 1E EA 2B 22 76 0C D0 
    00 02 92 1E 0C D0 18 02 92 0F 19 69 AD 5C 0C D0 B4 DC A4 5D 92 06 30 FF 
    0C D0 01 56 A5 00 92 06 30 FF 7E 07 A9 8A C4 06 C5 1E 0C D0 01 02 92 07 
    0C D0 92 1E 0C D0 18 02 92 0F E9 66 1F 76 A0 02 3E 92 F2 96 00 B6 F2 0E 
    3F 88 01 09 30 FF 42 1E 44 C3 A6 06 40 76 CB 9C 10 D0 92 1E 01 29 F2 5C 
    1F 76 A0 02 00 BE 03 56 3F 04 01 DC 42 A8 44 C2 40 76 CB 9C 0E D0 92 1E 
    AD 5C B4 DC A4 0E 7C 1E 10 D0 5E CC FF 0F A9 0E 92 0F 05 67 EA 28 F7 01 
    EF FF F6 02 16 02 42 1E 7C 8A 10 02 40 76 24 A2 4E 0F 05 61 EA 28 F5 01 
    EF FF EA 02 1F 76 A0 02 3A 8A D4 18 FE FF 3A 8A D4 18 FD FF 54 92 E2 96 
    E2 92 C3 FF E2 CA FF 90 E2 96 E2 92 54 96 51 92 E2 96 E2 92 C3 FF E2 CA 
    FF 90 E2 96 E2 92 51 96 53 92 E2 96 E2 92 C3 FF E2 CA FF 90 E2 96 E2 92 
    53 96 00 8F 44 01 A9 A8 3A 07 A9 8A C4 CC F8 FF 05 50 A9 88 00 8F 44 01 
    A9 A8 3A 07 A9 8A C4 7E 0E D0 92 C4 58 0E 42 C2 40 76 F5 9F 78 1E 1F 76 
    A0 02 00 8F 20 01 78 88 A9 A8 3A 07 A9 8A C4 7E 0E D0 92 06 42 1E 56 06 
    40 76 F5 9F 1F 76 A0 02 00 8F 22 01 A6 1E A9 A8 3A 07 A9 8A C4 C2 0E D0 
    92 C4 61 92 FF 90 A9 0E 42 C2 40 76 F5 9F 0A D0 92 1E 01 3B 1F 76 A0 02 
    00 8F 10 01 0A D0 28 FF FF FF 42 1E A9 A8 3A 07 A9 8A 92 06 40 76 90 9F 
    00 52 03 61 00 9A 03 6F A9 28 00 02 EA 96 0E D0 92 C4 5F CC 00 FF C7 FF 
    A9 0E 42 C2 40 76 F5 9F 78 1E 1F 76 A0 02 00 8F 14 01 A9 A8 3A 07 A9 8A 
    78 80 C4 92 A7 38 00 8F 14 01 A9 88 A9 A8 3A 07 A9 8A C4 7E 0E D0 92 C4 
    5D CC 00 FF C7 FF A9 0E 42 C2 40 76 F5 9F 0A D0 92 1E 01 3B 1F 76 A0 02 
    00 8F 16 01 0A D0 2F FF FE FF 42 1E A9 A8 3A 07 A9 8A 92 06 40 76 90 9F 
    00 52 05 61 EA 92 03 60 00 9A 03 6F A9 28 00 02 EA 96 22 76 0E D0 92 C4 
    60 CC 00 FF C7 FF A9 0E 42 C2 40 76 F5 9F 78 1E 1F 76 A0 02 00 8F 1A 01 
    A9 A8 3A 07 A9 8A 78 80 C4 92 A7 38 00 8F 1A 01 A9 88 A9 A8 3A 07 A9 8A 
    C4 7E 63 CC 00 FF C7 FF 00 8F 08 01 A9 80 A9 A8 3A 07 A9 8A C4 92 A7 38 
    00 8F 08 01 A9 88 A9 A8 3A 07 A9 8A C4 7E 40 8F 08 01 00 8F 08 01 63 CC 
    FF 00 A9 88 A9 A8 3A 07 A9 8A A9 A0 3A 07 A9 83 C4 93 A5 8A A6 92 A8 3C 
    C4 97 00 8F 0C 01 64 CC 00 FF C7 FF A9 80 A9 A8 3A 07 A9 8A C4 92 A7 38 
    00 8F 0C 01 A9 88 A9 A8 3A 07 A9 8A C4 7E 00 8F 0C 01 40 8F 0C 01 64 CC 
    FF 00 A9 88 A9 A8 3A 07 A9 8A A9 A0 3A 07 A9 83 C4 93 A5 8A A6 92 A8 3C 
    C4 97 00 8F 0E 01 62 CC FF 0F A9 88 A9 A8 3A 07 A9 8A A6 92 A9 CC FF 0F 
    A9 88 C4 CD 00 F0 A6 99 00 8F 0E 01 A9 A8 3A 07 A9 8A C4 7E 00 8F 0E 01 
    62 CC 00 F0 CB FF A9 88 A9 A8 3A 07 A9 8A C4 CC FF 0F A9 80 00 8F 0E 01 
    03 56 A6 0C A7 CA A9 88 A9 A8 3A 07 A9 8A C4 7E 00 8F 0A 01 5E CC 00 F0 
    CB FF A9 88 A9 A8 3A 07 A9 8A C4 CC FF 0F A9 80 00 8F 0A 01 03 56 A6 0C 
    A7 CA A9 88 A9 A8 3A 07 A9 8A C4 7E 00 8F 10 01 61 CC 00 FF C7 FF A9 80 
    A9 A8 3A 07 A9 8A C4 92 A7 38 00 8F 10 01 A9 88 A9 A8 3A 07 A9 8A C4 7E 
    0A D0 5F 92 FF 90 A9 0E 92 1E 01 3B 0A D0 28 FF FF FF 00 8F 12 01 42 1E 
    A9 A8 3A 07 A9 8A 92 06 40 76 90 9F 00 52 05 61 EA 92 03 60 00 9A 03 6F 
    A9 28 00 02 EA 96 00 8F 34 01 1F 76 A0 02 A9 A8 3A 07 A9 8A 5A CC FF 0F 
    A9 88 C4 CD 00 F0 A6 99 00 8F 34 01 A9 A8 3A 07 A9 8A C4 7E 5B 0E 78 1E 
    00 8F 35 01 A9 A8 3A 07 A9 8A 78 CC FF 01 A9 88 C4 CD 00 FE A6 99 00 8F 
    35 01 A9 A8 3A 07 A9 8A C4 7E 00 8F 36 01 A9 A8 3A 07 A9 8A 57 CC FF 0F 
    A9 88 C4 CD 00 F0 A6 99 00 8F 36 01 A9 A8 3A 07 A9 8A C4 7E 54 0E 78 1E 
    00 8F 37 01 A9 A8 3A 07 A9 8A 78 CC FF 01 A9 88 C4 CD 00 FE A6 99 00 8F 
    37 01 A9 A8 3A 07 A9 8A C4 7E 00 8F 39 01 A9 A8 3A 07 A9 8A C4 18 00 FE 
    0A D0 5C 0E 01 19 92 1E 00 02 0A D0 00 8F 3C 01 80 19 42 1E A9 A8 3A 07 
    A9 8A 92 06 40 76 90 9F 00 52 05 61 EA 92 03 60 00 9A 03 6F A9 28 00 02 
    EA 96 00 8F 3E 01 1F 76 A0 02 00 BE 40 8F 00 45 A9 A8 3A 07 42 C2 A9 8A 
    A9 A0 40 76 90 9F 00 52 05 61 EA 92 03 60 00 9A 03 6F A9 28 00 02 EA 96 
    1F 76 A0 02 32 02 3A 07 A9 8A C4 28 55 AA 50 CC 00 FF C7 FF A9 88 40 02 
    3A 07 A9 8A A6 CC 0F 00 A9 88 C4 CD F0 FF A6 99 40 02 3A 07 A9 8A C4 7E 
    0A D0 54 0E 92 1E 0A D0 92 06 0A D0 3F FF 92 1E A9 28 FF FF A8 28 00 FE 
    0A D0 42 1E 42 02 3A 07 A9 8A 92 06 40 76 90 9F 00 52 05 61 EA 92 03 60 
    00 9A 03 6F A9 28 00 02 EA 96 0A D0 51 0E 92 1E 01 3B 1F 76 A0 02 0A D0 
    29 FF FF FF 42 1E 42 02 3A 07 A9 8A 92 06 40 76 90 9F 00 52 05 61 EA 92 
    03 60 00 9A 03 6F A9 28 00 02 EA 96 53 0E 78 1E 1F 76 A0 02 45 02 3A 07 
    A9 8A 78 CC FF 01 A9 88 C4 CD 00 FE A6 99 45 02 3A 07 A9 8A C4 7E 00 BE 
    46 02 3A 07 A9 8A C4 C2 80 02 3A 07 A9 8A 41 8F 04 01 C4 A0 82 02 3A 07 
    A9 8A 40 8F 03 01 C4 A0 84 02 3A 07 A9 8A C4 18 F8 FF 86 02 3A 07 A9 8A 
    C4 18 80 FF 52 CC 00 FF C7 FF A9 88 48 02 3A 07 A9 8A A6 CC 1F 00 87 FF 
    A9 88 C4 CD FF E0 A6 99 48 02 3A 07 A9 8A C4 7E 0A D0 52 92 FF 90 A9 0E 
    92 1E 00 02 0A D0 20 19 42 1E 48 02 3A 07 A9 8A 92 06 40 76 90 9F 00 52 
    05 61 EA 92 03 60 00 9A 03 6F A9 28 00 02 EA 96 4F CC 00 FF 1F 76 A0 02 
    C7 FF A9 88 4A 02 3A 07 A9 8A C4 CC FF 0F A9 80 03 56 A6 0C A7 CA A9 88 
    4A 02 3A 07 A9 8A C4 7E 4F CC FF 00 A9 88 4C 02 3A 07 A9 8A A6 92 1F 90 
    A9 88 C4 CD E0 FF A6 99 4C 02 3A 07 A9 8A C4 7E 5D CC FF 00 A9 80 54 02 
    3A 07 A9 8A 54 02 3A 07 A6 1E C4 93 A6 8A A7 92 A8 3C C4 97 82 02 3A 07 
    A9 8A 40 8F 03 01 C4 A0 80 02 3A 07 A9 8A 41 8F 04 01 C4 A0 32 02 3A 07 
    A9 8A C4 2B 00 02 00 8F 44 01 1F 76 A0 02 08 19 42 1E A9 A8 3A 07 A9 8A 
    02 02 40 76 90 9F 00 52 05 61 EA 92 03 60 00 9A 07 6F EA 92 03 61 EA 92 
    03 6F A9 28 00 02 EA 96 1A 76 EA 92 CC FE BE 86 06 00 1C FE 44 1E 00 8F 
    DC 9F 1F 76 A1 02 00 A8 40 76 F7 9C 20 FF 00 72 40 76 23 9D 20 FF 00 72 
    40 76 7F A2 53 96 20 FF 00 72 53 5C 40 76 EB A1 AD 5C AD 5D 92 DC 90 DD 
    A4 5C A5 5D 40 76 FD 99 51 96 0F 52 E1 FF 97 00 1F 76 A0 02 32 28 00 10 
    A9 28 78 56 A8 28 34 12 34 1E 36 28 00 10 00 02 38 1E 30 2B 51 92 0A 52 
    1C 60 01 29 4F 25 50 AF 5C 1E 4D 25 4E AF 5A 1E 4B 25 4C AF 58 1E 49 25 
    4A AF 56 1E AD 5C 9C DC A4 5C 40 76 4D 98 40 76 DE 9D 02 52 53 60 1F 76 
    A0 02 32 28 00 60 4E 6F 0B 52 1C 60 01 29 4F 25 50 AF 5C 1E 4D 25 4E AF 
    5A 1E 4B 25 4C AF 58 1E 49 25 4A AF 56 1E AD 5C 9C DC A4 5C 40 76 99 98 
    40 76 01 9E 02 52 36 60 1F 76 A0 02 32 28 00 60 31 6F A9 28 00 01 51 54 
    0E 60 44 06 40 76 41 9A 46 1E 1F 76 A0 02 A9 28 00 10 32 54 23 60 46 06 
    34 1E 20 6F A9 28 00 03 51 54 0A 60 50 0E 56 1E 4F 0E 58 1E 42 1E 56 06 
    40 76 47 93 13 6F A9 28 00 05 51 54 04 60 40 76 CE 8C 0C 6F 51 92 0E 52 
    07 60 01 29 4F 25 50 AF 46 1E 46 06 26 6F 32 28 00 50 1F 76 A0 02 BF 56 
    41 0C 36 92 00 8F 34 A8 40 8F 38 A8 42 96 32 93 51 92 40 76 E5 98 00 52 
    F1 60 AD 5C AD 5D 92 DC 90 DD A4 5C A5 5D 40 76 FD 99 51 96 0F 52 E0 FF 
    6D FF 22 76 40 76 F9 A2 40 76 3E A2 1A 76 00 6F 9C FE 06 00 
    00 08 00 00 00 88 3A FE 70 97 6F 96 56 A0 54 A8 71 2B 05 8F 90 F8 58 A8 
    1F 76 A0 02 A0 02 3A 07 5A 1E 7F 92 72 96 3C 92 73 96 3D 92 74 96 00 02 
    5C 1E 5E 1E 60 1E 62 1E 64 1E 03 56 6F 01 75 96 70 92 76 96 56 06 66 1E 
    7E 06 68 1E 77 2B 78 2B 79 2B 00 02 6A 1E 7A 2B 6C 1E 6E 1E 54 06 46 1E 
    05 8F 00 F8 52 A8 3A 06 52 0F E0 FF 31 02 22 76 40 76 FA A1 01 52 03 60 
    BF 56 71 01 71 92 E0 FF BA 00 07 8F 00 80 A9 A8 46 0F 21 66 07 8F 00 84 
    A9 A8 46 0F 1C 69 00 02 1F 76 A0 02 08 19 42 1E 28 02 3A 07 A9 8A 00 02 
    40 76 90 9F 00 52 03 61 00 9A 03 6F A9 28 00 02 71 96 72 92 E1 FF 9B 00 
    03 52 E1 FF 98 00 72 2B EF FF 95 00 07 8F 00 84 A9 A8 46 0F 19 66 07 8F 
    00 88 A9 A8 46 0F 14 69 00 02 1F 76 A0 02 08 19 42 1E 28 02 3A 07 A9 8A 
    01 02 40 76 90 9F 00 52 03 61 00 9A 03 6F A9 28 00 02 71 96 77 6F 07 8F 
    00 88 A9 A8 46 0F 19 66 07 8F 00 8C A9 A8 46 0F 14 69 00 02 1F 76 A0 02 
    08 19 42 1E 28 02 3A 07 A9 8A 02 02 40 76 90 9F 00 52 03 61 00 9A 03 6F 
    A9 28 00 02 71 96 5A 6F 08 8F 00 00 A9 A8 46 0F 19 66 09 8F 00 00 A9 A8 
    46 0F 14 69 00 02 1F 76 A0 02 08 19 42 1E 28 02 3A 07 A9 8A 00 02 40 76 
    90 9F 00 52 03 61 00 9A 03 6F A9 28 00 02 71 96 3D 6F 09 8F 00 00 A9 A8 
    46 0F 19 66 0A 8F 00 00 A9 A8 46 0F 14 69 00 02 1F 76 A0 02 08 19 42 1E 
    28 02 3A 07 A9 8A 01 02 40 76 90 9F 00 52 03 61 00 9A 03 6F A9 28 00 02 
    71 96 20 6F 0A 8F 00 00 A9 A8 46 0F 19 66 0B 8F 00 00 A9 A8 46 0F 14 69 
    00 02 1F 76 A0 02 08 19 42 1E 28 02 3A 07 A9 8A 02 02 40 76 90 9F 00 52 
    03 61 00 9A 03 6F A9 28 00 02 71 96 03 6F 71 28 FA 01 72 92 09 61 01 52 
    07 61 02 52 05 61 03 52 03 61 71 28 FF 01 46 06 30 FF 4A 1E 73 0E 01 19 
    4A CE 49 CF 5C 1E 72 92 02 52 0A 61 75 92 06 61 73 88 75 0E 5C 07 A6 0F 
    03 69 71 28 FC 01 72 92 01 52 0E 61 00 52 0C 61 76 92 08 61 5C 06 74 88 
    01 29 42 FF 76 0D A6 0F 03 69 71 28 FD 01 72 92 03 52 0E 60 75 92 07 90 
    0B 61 76 0E A6 1E 75 92 C2 FF A9 80 A6 06 A7 0F 03 61 71 28 FE 01 07 02 
    07 8F 41 02 C4 89 6E 1E 06 02 6E 0F 0E 60 0A 8F 00 00 A9 A8 46 0F 09 66 
    0B 8F 00 00 A9 A8 46 0F 04 69 71 28 FA 01 10 6F 05 02 6E 0F 0D 60 08 8F 
    00 80 A9 A8 46 0F 06 66 09 8F 00 80 A9 A8 46 0F 03 66 71 28 FA 01 07 8F 
    00 80 A9 A8 46 0F 06 66 07 8F 08 80 A9 A8 46 0F 0B 66 07 8F 00 82 A9 A8 
    46 0F 0E 66 07 8F 08 82 A9 A8 46 0F 09 69 72 92 02 52 04 60 71 28 FF 01 
    03 6F BF 56 72 01 71 92 E0 FF EC 00 10 9A 40 76 12 97 02 9A 40 76 3E 9F 
    22 76 72 92 16 60 A9 28 FF FF A8 28 FF FE 1F 76 A0 02 42 1E 8E 02 3A 07 
    A9 8A 2F FF 00 02 40 76 90 9F 00 52 03 61 00 9A 03 6F A9 28 00 02 71 96 
    00 BE 88 02 1F 76 A0 02 3A 07 42 C2 A9 8A 4A 06 40 76 90 9F 00 52 05 61 
    71 92 03 60 00 9A 03 6F A9 28 00 02 71 96 00 52 E0 FF 97 00 72 92 02 52 
    1D 61 5C 06 01 29 40 FF 6C 1E 6F 0E 6C 07 01 19 5E 1E 6C 06 64 1E 5E 06 
    64 0F 10 68 66 C5 64 06 58 07 A9 8A C7 92 C4 96 01 02 66 07 66 1E 01 02 
    64 07 64 1E 5E 06 64 0F F2 67 8F 02 1F 76 A0 02 3A 07 A9 8A C4 CC 00 01 
    C7 FF 01 52 6A 61 72 92 01 52 67 61 5C 06 01 29 42 FF 60 1E 76 0E 60 07 
    62 1E 08 8F 00 00 A9 A8 46 0F 0E 66 0B 8F 00 00 A9 A8 46 0F 09 69 4A 06 
    0F FF 20 00 43 FF 1F FF 10 02 6A 1E 12 6F 07 8F 00 80 A9 A8 46 0F 0D 66 
    07 8F 00 8C A9 A8 46 0F 08 69 4A 06 0F FF 1E 00 43 FF 1C FF 71 10 6A 1E 
    71 92 3B 60 7A 2B 60 06 64 1E 62 06 64 0F 35 69 6A 06 4E 1E 4E C5 C7 92 
    77 96 64 06 0F 60 68 C5 C7 92 78 96 77 92 C7 FF A9 88 5A 8A 03 56 78 08 
    A6 CA CC 96 BF 56 7A 01 1A 6F 01 02 64 0F 17 60 68 8A C4 92 C7 FF 79 96 
    01 02 68 07 68 1E 7A 92 01 52 08 60 5A 8A 03 56 78 08 79 CA CC 96 7A 2B 
    06 6F 5A 8A 03 56 77 08 79 CA CC 96 01 02 64 07 64 1E 62 06 64 0F CD 66 
    02 9A 40 76 12 97 22 76 8F 02 1F 76 A0 02 3A 07 A9 8A C4 CC 00 01 C7 FF 
    01 52 17 60 A9 28 FF FF A8 28 FF FE 42 1E 8E 02 3A 07 A9 8A 00 02 40 76 
    90 9F 00 52 05 61 71 92 03 60 00 9A 05 6F 71 92 03 60 A9 28 00 02 71 96 
    1A 76 03 6F 71 28 03 02 71 92 BA FE 06 00 BD B2 BD AA AD 5A 86 DA AD 08 
    A8 00 1B D0 92 2B 1A D0 92 2B 19 D0 92 2B 16 D0 92 2B 15 D0 92 2B A9 28 
    00 10 1F 76 A0 02 32 54 06 61 15 D0 92 92 15 D0 01 9C 92 96 1B D0 92 2B 
    1B D0 92 92 20 52 0F 67 00 8F 00 A8 1B D0 92 58 94 2B 1B D0 92 92 1B D0 
    01 9C 92 96 1B D0 92 92 20 52 F5 68 40 76 5A 9F 1F 76 A1 02 00 C5 67 3E 
    48 96 22 76 EF FF 26 02 40 76 6A A1 46 1E 1B D0 92 2B EF FF 13 02 80 52 
    39 67 1A D0 92 2B 1A 6F 1F 76 A1 02 00 C5 67 3E 17 D0 92 96 AD 5C A4 08 
    76 FF 1A D0 92 59 A4 5C 17 D0 92 92 9C 96 1B D0 92 92 1B D0 01 9C 92 96 
    1A D0 92 92 1A D0 01 9C 92 96 48 92 1A D0 92 54 E4 66 1A D0 92 96 1A D0 
    92 92 80 52 73 67 AD 5C A4 08 76 FF 1A D0 92 58 A4 5C 94 28 FF FF 1A D0 
    92 92 1A D0 01 9C 92 96 1A D0 92 92 80 52 F0 68 61 6F 1B D0 92 9E 80 52 
    3A 67 1A D0 92 2B 15 6F 1F 76 A1 02 00 C5 67 3E 17 D0 92 96 AD 5C A4 08 
    76 FF 1A D0 92 59 A4 5C 17 D0 92 92 9C 96 1A D0 92 92 1A D0 01 9C 92 96 
    48 92 1B D0 92 9E 1A D0 92 54 E7 66 1A D0 92 92 1B D0 92 94 1B D0 92 96 
    1A D0 92 92 80 52 36 67 AD 5C A4 08 76 FF 1A D0 92 58 A4 5C 94 28 FF FF 
    1A D0 92 92 1A D0 01 9C 92 96 1A D0 92 92 80 52 F0 68 24 6F 1A D0 92 2B 
    1A D0 92 92 80 52 1E 67 1F 76 A1 02 00 C5 67 3E 17 D0 92 96 AD 5C A4 08 
    76 FF 1A D0 92 59 A4 5C 17 D0 92 92 9C 96 1B D0 92 92 1B D0 01 9C 92 96 
    1A D0 92 92 1A D0 01 9C 92 96 1A D0 92 92 80 52 E4 68 19 D0 92 2B 19 D0 
    92 92 10 52 E7 FF 6C 01 AD 5C A4 08 76 FF 19 D0 03 56 92 03 A9 58 A4 5C 
    94 92 1C D0 92 96 AD 5C A4 08 76 FF 19 D0 03 56 92 03 A9 58 A4 5C 01 D8 
    94 92 1D D0 92 96 AD 5C A4 08 76 FF 19 D0 03 56 92 03 A9 58 A4 5C 02 D8 
    94 92 1E D0 92 96 AD 5C A4 08 76 FF 19 D0 03 56 92 03 A9 58 A4 5C 03 D8 
    94 92 1F D0 92 96 AD 5C A4 08 76 FF 19 D0 03 56 92 03 A9 58 A4 5C 04 D8 
    94 92 20 D0 92 96 AD 5C A4 08 76 FF 19 D0 03 56 92 03 A9 58 A4 5C 05 D8 
    94 92 21 D0 92 96 AD 5C A4 08 76 FF 19 D0 03 56 92 03 A9 58 A4 5C 06 D8 
    94 92 22 D0 92 96 AD 5C A4 08 76 FF 19 D0 03 56 92 03 A9 58 A4 5C 07 D8 
    94 92 23 D0 92 96 48 92 16 D0 92 54 E9 FF F6 00 15 D0 92 92 69 60 46 06 
    40 76 00 80 4A 1E A9 28 EF BE A8 28 AD DE 4A 0F 5F 61 4A 06 40 76 FF A2 
    18 D0 92 96 18 9A 40 76 8A 9E 09 D0 92 96 40 76 FA A1 02 52 FD 60 09 D0 
    92 92 14 61 1F 76 A0 02 32 28 00 22 00 02 34 1E 09 D0 92 92 40 76 2C 99 
    1F 76 A0 02 00 02 38 1E 15 D0 92 92 15 D0 01 9C 92 96 15 D0 92 92 38 60 
    4A 8A 06 9A 40 76 60 94 09 D0 92 96 40 76 FA A1 02 52 FD 60 40 76 DD A2 
    0A D0 92 1E AD 5D A5 08 5E FF 18 D0 4A 8A 92 0E A5 5D 40 76 84 8F 09 D0 
    92 96 09 D0 92 92 04 60 0A D0 92 06 19 61 15 D0 92 92 11 60 1F 76 A0 02 
    32 28 00 20 0C D0 92 06 34 1E 09 D0 92 92 40 76 2C 99 0A D0 1F 76 A0 02 
    92 06 38 1E 15 D0 92 92 15 D0 01 9C 92 96 15 D0 92 92 34 60 AD 5D 00 02 
    42 1E 43 2B A5 08 6E FF 08 9A 00 9B 46 8A A5 5D 40 76 00 88 09 D0 92 96 
    40 76 FA A1 01 52 FD 61 40 76 DD A2 0A D0 92 1E 09 D0 92 92 04 60 0A D0 
    92 06 18 61 15 D0 92 92 10 60 1F 76 A0 02 32 28 00 40 46 06 34 1E 09 D0 
    92 92 40 76 2C 99 0A D0 1F 76 A0 02 92 06 38 1E 15 D0 92 92 15 D0 01 9C 
    92 96 1A D0 92 2B 1A D0 92 92 08 52 4E 67 AD 5C A4 08 6E FF 1A D0 92 58 
    A4 5C 01 D8 94 0E F2 1E F2 06 3F FF F2 1E AD 5C A4 08 6E FF 1A D0 92 58 
    A4 5C F2 06 94 AF F2 1E 15 D0 92 92 2D 60 AD 5C AD 5D A4 08 5E FF A5 08 
    58 FF 1A D0 A4 0E 42 1E A5 5D 92 0E 46 07 A9 8A 01 02 40 76 DC A1 09 D0 
    92 96 09 D0 92 92 18 61 15 D0 92 92 10 60 1F 76 A0 02 32 28 00 30 0C D0 
    92 06 34 1E 09 D0 92 92 40 76 2C 99 1F 76 A0 02 00 02 38 1E 15 D0 92 92 
    15 D0 01 9C 92 96 1A D0 92 92 1A D0 02 9C 92 96 1A D0 92 92 08 52 B4 68 
    08 02 46 07 46 1E 16 D0 92 92 16 D0 08 9C 92 96 19 D0 92 92 19 D0 01 9C 
    92 96 19 D0 92 92 10 52 E8 FF 98 FE 40 76 5A 9F 1B D0 92 92 1B D0 92 96 
    48 92 1B D0 92 54 E6 FF EC FD 1F 76 A1 02 00 C5 67 3E 48 96 16 D0 92 2B 
    00 52 E0 FF DB FD 1A 76 AD 08 58 FF BE 86 BE 8B 06 00 BD B2 BD AA AD 5A 
    86 DA AD 08 9C 00 1F 76 A0 02 32 28 00 10 A9 28 78 65 A8 28 34 12 34 1E 
    13 D0 92 2B 12 D0 92 2B 00 8F DC 9F 1F 76 A1 02 00 A8 40 76 DC 9F A9 88 
    20 FF AA 08 A6 0F 08 61 1F 76 A0 02 32 28 00 30 08 8F 00 00 34 A8 40 76 
    CC A1 40 76 6A A1 40 76 5A 9F 1F 76 A1 02 00 C5 67 3E 46 96 22 76 EF FF 
    58 01 40 76 6A A1 44 1E 16 D0 92 2B EF FF 45 01 80 52 39 67 15 D0 92 2B 
    1A 6F 1F 76 A1 02 00 C5 67 3E 17 D0 92 96 AD 5C A4 08 7A FF 15 D0 92 59 
    A4 5C 17 D0 92 92 9C 96 16 D0 92 92 16 D0 01 9C 92 96 15 D0 92 92 15 D0 
    01 9C 92 96 46 92 15 D0 92 54 E4 66 15 D0 92 96 15 D0 92 92 80 52 73 67 
    AD 5C A4 08 7A FF 15 D0 92 58 A4 5C 94 28 FF FF 15 D0 92 92 15 D0 01 9C 
    92 96 15 D0 92 92 80 52 F0 68 61 6F 16 D0 92 9E 80 52 3A 67 15 D0 92 2B 
    15 6F 1F 76 A1 02 00 C5 67 3E 17 D0 92 96 AD 5C A4 08 7A FF 15 D0 92 59 
    A4 5C 17 D0 92 92 9C 96 15 D0 92 92 15 D0 01 9C 92 96 46 92 16 D0 92 9E 
    15 D0 92 54 E7 66 15 D0 92 92 16 D0 92 94 16 D0 92 96 15 D0 92 92 80 52 
    36 67 AD 5C A4 08 7A FF 15 D0 92 58 A4 5C 94 28 FF FF 15 D0 92 92 15 D0 
    01 9C 92 96 15 D0 92 92 80 52 F0 68 24 6F 15 D0 92 2B 15 D0 92 92 80 52 
    1E 67 1F 76 A1 02 00 C5 67 3E 17 D0 92 96 AD 5C A4 08 7A FF 15 D0 92 59 
    A4 5C 17 D0 92 92 9C 96 16 D0 92 92 16 D0 01 9C 92 96 15 D0 92 92 15 D0 
    01 9C 92 96 15 D0 92 92 80 52 E4 68 14 D0 92 2B 14 D0 92 92 20 52 E7 FF 
    9E 00 AD 5C A4 08 7A FF 14 D0 03 56 92 02 A9 58 A4 5C 94 92 18 D0 92 96 
    AD 5C A4 08 7A FF 14 D0 03 56 92 02 A9 58 A4 5C 01 D8 94 92 19 D0 92 96 
    AD 5C A4 08 7A FF 14 D0 03 56 92 02 A9 58 A4 5C 02 D8 94 92 1A D0 92 96 
    AD 5C A4 08 7A FF 14 D0 03 56 92 02 A9 58 A4 5C 03 D8 94 92 1B D0 92 96 
    46 92 12 D0 92 54 58 69 40 76 FA A1 01 52 FD 61 15 D0 92 2B 15 D0 92 92 
    04 52 4E 67 AD 5C A4 08 76 FF 15 D0 92 58 A4 5C 01 D8 94 0E F2 1E F2 06 
    3F FF F2 1E AD 5C A4 08 76 FF 15 D0 92 58 A4 5C F2 06 94 AF F2 1E 13 D0 
    92 92 2D 60 AD 5C AD 5D A4 08 68 FF A5 08 64 FF 15 D0 A4 0E 42 1E A5 5D 
    92 0E 44 07 A9 8A 01 02 40 76 DC A1 09 D0 92 96 09 D0 92 92 18 61 13 D0 
    92 92 10 60 1F 76 A0 02 32 28 00 30 0A D0 92 06 34 1E 09 D0 92 92 40 76 
    2C 99 1F 76 A0 02 00 02 38 1E 13 D0 92 92 13 D0 01 9C 92 96 15 D0 92 92 
    15 D0 02 9C 92 96 15 D0 92 92 04 52 B4 68 04 02 44 07 44 1E 12 D0 92 92 
    12 D0 04 9C 92 96 14 D0 92 92 14 D0 01 9C 92 96 14 D0 92 92 20 52 E8 FF 
    66 FF 40 76 5A 9F 16 D0 92 92 16 D0 92 96 46 92 16 D0 92 54 E6 FF BA FE 
    1F 76 A1 02 00 C5 67 3E 46 96 12 D0 92 2B 00 52 E0 FF A9 FE 1A 76 AD 08 
    64 FF BE 86 BE 8B 06 00 16 FE 46 1E 56 2B 03 8F 00 00 00 90 03 91 A4 0F 
    06 69 00 8F 2A A9 F7 02 40 76 EB A2 46 06 AB 2B AA 28 00 80 00 90 A8 18 
    00 C0 AB 0F 14 61 46 06 AA 28 00 40 00 90 A8 18 00 C0 AB 0F 0C 61 46 06 
    00 90 A8 18 00 C0 58 FF 06 61 00 8F 2A A9 FA 02 40 76 EB A2 40 76 96 A2 
    00 52 04 61 56 2B EF FF F0 00 22 76 05 8F 0E D2 C4 18 FD FF 1A 76 17 02 
    40 76 58 02 05 8F 08 D2 C4 92 03 90 53 96 05 8F 32 D2 C4 92 02 90 55 96 
    46 06 03 91 A8 0E 48 1E 55 92 53 CA A9 0E 48 0F 12 61 22 76 05 8F 0E D2 
    C4 18 FE FF 1A 76 0C 02 40 76 58 02 46 06 00 90 03 91 40 76 00 98 0B 02 
    40 76 58 02 01 9A 40 76 AA 9F AB 2B AA 28 00 80 46 06 00 90 A8 18 00 C0 
    AB 0F 09 61 46 06 AA 28 00 40 00 90 A8 18 00 C0 AB 0F 77 60 46 06 00 9B 
    FF 90 4A 1E AC 28 12 00 46 06 00 90 7C 91 22 56 AC 28 18 00 3B 56 4A 98 
    49 99 AC 28 17 00 46 06 00 90 A8 18 80 0F 22 56 3F FF 4A 98 49 99 05 8F 
    14 D2 C4 06 00 9B FF 90 4C 1E C4 06 00 90 A8 18 00 1F 4C 98 4B 99 C4 06 
    00 90 1F 91 4C 98 4B 99 05 8F 0E D2 C4 92 01 90 52 96 4A 06 4C 0F 04 60 
    52 92 01 52 3F 61 22 76 C4 18 FE FF 1A 76 0C 02 40 76 58 02 22 76 05 8F 
    14 D2 4A 06 C4 1E 05 8F 0E D2 C4 1A 01 00 AC 28 12 00 46 06 00 90 7C 91 
    22 56 50 1E 01 02 50 07 39 FF 4E 1E 05 8F 16 D2 C4 92 01 90 54 96 07 6F 
    C4 92 01 90 54 96 01 02 41 56 4E 00 54 92 01 52 03 61 4E 06 F6 60 1A 76 
    46 06 00 90 03 91 42 1E 46 06 FF 90 A8 18 FC 0F 44 1E 46 06 00 90 A8 18 
    00 30 40 76 00 90 56 96 14 6F BF 56 56 01 11 6F 46 06 00 90 A8 18 00 C0 
    58 FF 0B 60 22 76 05 8F 0E D2 C4 18 FE FF 2D F6 00 77 1A 76 BF 56 56 01 
    56 92 25 61 46 CC 00 7F C7 FF 51 96 7E 52 05 60 69 FF 40 76 AA 9F 05 6F 
    02 9C 69 FF 40 76 AA 9F 46 06 AB 2B AA 28 00 80 00 90 A8 18 00 C0 AB 0F 
    07 60 22 76 05 8F 0E D2 C4 1A 02 00 1A 76 28 02 40 76 58 02 51 92 40 76 
    AA 9F 02 6F 25 76 56 92 69 FF 96 FE 06 00 16 FE 4E A0 4C 1E 4A A8 51 2B 
    00 02 01 19 50 1E 4A 06 48 1E 4C 06 42 1E 48 06 40 76 FD 9A 01 52 67 60 
    22 76 20 02 1F 76 A0 02 3A 07 A9 8A C4 06 54 1E 20 02 3A 07 A9 8A AB 28 
    FF FF AA 28 05 05 C4 A9 00 8F 80 01 A9 A8 3A 07 A9 8A C4 CC 02 00 C0 FF 
    55 96 00 02 00 8F 80 01 03 19 42 1E A9 A8 3A 07 A9 8A 02 02 40 76 90 9F 
    00 52 03 61 00 9A 03 6F A9 28 00 02 51 96 1A 76 40 76 04 9F 51 92 13 60 
    AD 5C 90 DC A4 0E 42 1E 43 2B 4E 83 4A 8A 4C 06 40 76 5A 95 51 96 00 52 
    06 61 4E 8A 00 02 F4 1E 51 28 F4 01 22 76 20 02 54 C4 1F 76 A0 02 3A 07 
    A9 8A C4 C2 01 29 00 02 00 8F 80 01 03 19 42 1E A9 A8 3A 07 A9 8A 03 56 
    55 01 00 9B 02 90 40 76 90 9F 00 52 05 61 51 92 03 60 00 9A 05 6F 51 92 
    03 60 A9 28 00 02 51 96 1A 76 03 6F 51 28 FA 01 51 92 96 FE 06 00 
    00 08 00 00 00 90 1E FE 48 1E 48 06 17 61 2F FF 00 20 48 0F 13 61 20 FF 
    4B 03 00 8F 2A A9 40 76 EB A2 0C 6F BF 56 5D 02 1C 6F 5D 2B 1A 6F BF 56 
    5D 01 17 6F BF 56 5D 01 14 6F 62 C4 A6 06 F3 61 01 8F 00 00 A9 A8 A6 0F 
    F1 61 02 8F 00 00 A9 A8 A6 0F EE 61 03 8F 00 00 A9 A8 A6 0F E7 61 EB 6F 
    5E 2B 48 06 05 60 05 8F 00 E7 48 A8 04 6F 05 8F 40 E7 48 A8 64 06 00 9B 
    FF 90 4A 1E AC 28 17 00 64 06 00 90 A8 18 80 0F 22 56 4C 1E AC 28 12 00 
    64 06 00 90 7C 91 22 56 4E 1E 84 E2 4E 00 84 E2 4C 01 8F E8 02 E0 8F E8 
    09 E0 84 E2 4A 00 00 E7 51 00 40 76 D8 93 03 E2 50 00 84 E2 4C 01 84 E2 
    4E 00 8F E8 0A E0 8F E8 00 E0 84 E2 4A 01 00 E7 10 00 40 76 D8 93 03 E2 
    52 00 AF E2 50 00 11 E8 00 FC 14 AD 10 64 02 E8 B0 24 03 E2 56 00 8A E6 
    00 00 00 77 00 77 A9 BF 12 0F 0C 19 58 1E 18 02 5C 1E 29 6F AF E2 52 00 
    50 E8 00 00 00 77 90 E8 00 48 00 77 03 E2 54 00 01 E8 01 FC 50 E8 00 B2 
    40 76 D8 93 03 E2 56 00 AF E2 54 00 AF E2 56 01 20 E7 08 00 00 77 8A E6 
    00 00 00 77 03 E2 58 00 AF E2 54 00 8A E6 00 00 00 77 00 77 A9 BF 12 0F 
    30 FF 5C 1E AF E2 56 00 AF E2 50 01 00 E7 08 00 00 77 8A E6 00 00 00 77 
    03 E2 5A 00 05 8F 00 E7 A9 A8 48 0F 05 60 15 9A 40 76 2F A0 05 6F A9 28 
    15 01 40 76 2F A0 48 06 40 76 B4 A0 48 06 40 76 9F A0 48 06 40 76 08 A1 
    48 06 40 76 C9 A0 48 06 40 76 5D A0 5D 5C 48 06 40 76 AA 9E 5E 5C 48 06 
    40 76 C8 9E 58 06 42 1E 5C 06 44 1E 5A 06 46 1E 48 06 40 76 D4 95 00 8F 
    00 0A 48 06 40 76 96 9D 48 06 40 76 1C A1 14 02 48 07 A9 8A C4 92 03 90 
    FB 61 14 02 48 07 A9 8A 00 BE 00 9A C4 93 03 91 02 53 02 60 01 9A 00 52 
    02 61 01 BE A6 92 9E FE 06 00 00 9A 40 76 18 A0 A9 28 00 02 40 76 18 A0 
    A9 28 00 03 40 76 18 A0 A9 28 00 04 40 76 18 A0 A9 28 00 05 40 76 18 A0 
    A9 28 00 0D 40 76 18 A0 A9 28 00 0E 40 76 18 A0 A9 28 00 10 40 76 18 A0 
    A9 28 00 12 40 76 18 A0 A9 28 00 18 40 76 18 A0 02 9A 40 76 18 A0 A9 28 
    02 01 40 76 18 A0 A9 28 02 02 40 76 18 A0 A9 28 02 03 40 76 18 A0 A9 28 
    02 04 40 76 18 A0 A9 28 02 05 40 76 18 A0 A9 28 02 06 40 76 18 A0 A9 28 
    02 07 40 76 18 A0 03 9A 40 76 18 A0 A9 28 03 01 40 76 18 A0 A9 28 03 02 
    40 76 18 A0 04 9A 40 76 18 A0 A9 28 04 01 40 76 18 A0 06 9A 40 76 18 A0 
    A9 28 06 01 40 76 18 A0 07 9A 40 76 18 A0 A9 28 07 01 40 76 18 A0 08 9A 
    40 76 18 A0 A9 28 08 01 40 76 18 A0 09 9A 40 76 18 A0 A9 28 09 01 40 76 
    18 A0 0A 9A 40 76 18 A0 A9 28 0A 04 40 76 18 A0 0D 9A 40 76 18 A0 A9 28 
    0D 01 40 76 18 A0 A9 28 0D 02 40 76 18 A0 0E 9A 40 76 18 A0 A9 28 0E 01 
    40 76 18 A0 A9 28 0E 02 40 76 18 A0 A9 28 0E 03 40 76 18 A0 A9 28 10 10 
    40 76 18 A0 A9 28 10 11 40 76 18 A0 11 9A 40 76 18 A0 A9 28 11 01 40 76 
    18 A0 A9 28 11 02 40 76 18 A0 A9 28 11 03 40 76 18 A0 12 9A 40 76 18 A0 
    A9 28 12 01 40 76 18 A0 13 9A 40 76 18 A0 A9 28 13 01 40 76 18 A0 14 9A 
    40 76 18 A0 15 9A 40 76 18 A0 A9 28 15 01 40 76 18 A0 19 9A 40 76 18 A0 
    1A 9A 40 76 18 A0 1B 9A 40 76 18 A0 06 00 04 FE 44 1E 01 02 44 0F 27 60 
    08 8F 01 1A A9 A8 40 76 6F 9B 01 D4 1D 02 40 76 40 9C 00 02 42 1E 1D 02 
    40 76 68 97 03 D4 1D 02 40 76 A6 9B 08 8F 01 18 A9 A8 40 76 6F 9B 00 D4 
    1C 02 40 76 40 9C 00 02 42 1E 1C 02 40 76 68 97 03 D4 1C 02 40 76 A6 9B 
    EF FF A1 00 21 02 44 0F 26 60 08 8F 06 00 A9 A8 40 76 6F 9B 01 D4 10 02 
    40 76 40 9C 00 02 42 1E 10 02 40 76 68 97 03 D4 10 02 40 76 A6 9B 08 8F 
    06 02 A9 A8 40 76 6F 9B 00 D4 11 02 40 76 40 9C 00 02 42 1E 11 02 40 76 
    68 97 03 D4 11 02 40 76 A6 9B 78 6F 41 02 44 0F 26 60 06 8F 06 10 A9 A8 
    40 76 6F 9B 01 D4 08 02 40 76 40 9C 00 02 42 1E 08 02 40 76 68 97 03 D4 
    08 02 40 76 A6 9B 06 8F 06 12 A9 A8 40 76 6F 9B 00 D4 09 02 40 76 40 9C 
    00 02 42 1E 09 02 40 76 68 97 03 D4 09 02 40 76 A6 9B 50 6F 61 02 44 0F 
    26 60 06 8F 09 04 A9 A8 40 76 6F 9B 01 D4 02 02 40 76 40 9C 00 02 42 1E 
    02 02 40 76 68 97 03 D4 02 02 40 76 A6 9B 06 8F 09 06 A9 A8 40 76 6F 9B 
    00 D4 03 02 40 76 40 9C 00 02 42 1E 03 02 40 76 68 97 03 D4 03 02 40 76 
    A6 9B 28 6F 81 02 44 0F 25 60 08 8F 06 00 A9 A8 40 76 6F 9B 01 D4 10 02 
    40 76 40 9C 00 02 42 1E 10 02 40 76 68 97 03 D4 10 02 40 76 A6 9B 06 8F 
    09 06 A9 A8 40 76 6F 9B 00 D4 03 02 40 76 40 9C 00 02 42 1E 03 02 40 76 
    68 97 03 D4 03 02 40 76 A6 9B 84 FE 06 00 0E FE 4D 96 4C A8 4E 2B 4C 06 
    46 1E 05 8F 00 F8 4A A8 1F 76 A0 02 3A 06 4A 0F E0 FF 9D 00 22 76 00 8F 
    44 01 A9 A8 3A 07 A9 8A C4 CC F8 FF 05 50 A9 88 00 8F 44 01 A9 A8 3A 07 
    A9 8A C4 7E 01 3B 40 8F D0 07 2C FF FF FF 00 8F 36 01 42 1E A9 A8 3A 07 
    A9 8A A9 A0 40 76 90 9F 00 52 03 61 00 9A 03 6F A9 28 00 02 4E 96 00 8F 
    44 01 1F 76 A0 02 A9 A8 3A 07 A9 8A C4 CC F8 FF 02 50 A9 88 00 8F 44 01 
    A9 A8 3A 07 A9 8A C4 7E 1A 76 40 76 FA A1 01 52 03 60 BF 56 4E 01 4E 92 
    5F 60 46 06 40 76 B1 96 4E 96 00 52 59 60 46 06 30 FF 46 1E 10 9A 40 76 
    12 97 22 76 1F 76 A0 02 18 02 3A 07 A9 8A C4 1A 01 00 1A 02 3A 07 A9 8A 
    40 8F FF FF C4 A0 00 8F 44 01 A9 A8 3A 07 A9 8A C4 CC F8 FF 05 50 A9 88 
    00 8F 44 01 A9 A8 3A 07 A9 8A C4 7E 00 8F 60 01 4D 88 A9 A8 3A 07 A9 8A 
    C4 7E 00 8F 44 01 A9 A8 3A 07 A9 8A C4 CC F8 FF 02 50 A9 88 00 8F 44 01 
    A9 A8 3A 07 A9 8A C4 7E 1A 76 18 02 3A 07 A9 8A C4 18 FE FF 22 76 00 BE 
    88 02 3A 07 42 C2 A9 8A 46 06 40 76 90 9F 00 52 03 61 00 9A 03 6F A9 28 
    00 02 4E 96 1A 76 00 52 07 60 08 9A 40 76 12 97 03 6F 4E 28 03 02 4E 92 
    8E FE 06 00 12 FE 4A 1E 1F 76 A0 02 32 28 00 10 A9 28 78 56 A8 28 34 12 
    34 1E 4F 2B 51 2B 22 76 4A 92 5E FF 52 96 08 8F 00 00 4E A8 01 02 56 0F 
    05 60 09 8F 00 00 4E A8 07 6F 02 02 56 0F 04 60 0A 8F 00 00 4E A8 4E 8A 
    52 92 40 76 98 92 50 96 17 6F 20 FF D0 07 45 8F 48 F9 C5 0F 11 67 22 76 
    05 02 05 8F 44 F9 C4 1E 05 8F 36 F9 C4 06 A9 18 00 F0 C4 1E 02 02 05 8F 
    44 F9 C4 1E 1A 76 40 76 FA A1 02 52 E7 60 40 76 DD A2 4C 1E 50 92 03 60 
    4C 06 10 61 1F 76 A0 02 32 28 00 21 00 02 34 1E 50 92 40 76 2C 99 1F 76 
    A0 02 4C 06 38 1E BF 56 51 01 4F 2B 4F 92 10 52 34 63 01 BE 4A 06 00 9B 
    01 90 A6 0F 26 60 51 92 24 60 56 06 21 56 4F 00 00 8F A8 AA AD 5D 33 FF 
    AC 07 30 FF 01 56 A4 00 88 DD A5 5D 20 FF 00 08 C4 8A 40 76 84 8F 50 96 
    00 52 0F 61 1F 76 A0 02 32 28 00 20 48 06 34 1E 50 92 40 76 2C 99 1F 76 
    A0 02 00 02 38 1E 51 0A 4A 06 01 29 40 FF 4A 1E 4F 0A 4F 92 10 52 CE 64 
    1A 76 92 FE 06 00 BD 3A BD B2 BD AA BD A2 02 FE 01 29 A9 BF 12 0F 58 FF 
    5B 61 A8 5C 7F 91 A8 08 80 00 42 1E A4 93 D6 FF A8 5C A9 BF 16 0F 67 61 
    A8 5D 7F 91 A8 08 80 00 A8 59 A9 58 A5 93 D6 FF A8 5D A4 93 A5 71 A8 18 
    00 01 A6 97 A4 18 FF 00 A5 18 FF 00 7F DC A4 92 A5 9E A7 96 4D 64 A9 08 
    01 FF 3E 62 A1 93 A0 92 36 FF A8 59 A9 58 42 06 35 FF 0E F6 A1 1F A9 5B 
    A3 01 0A F6 A1 1F 2D 56 A2 04 A3 2D A0 36 40 FF 0B F6 A1 1F 33 FF 00 9B 
    30 FF 54 FF A2 0C A3 95 40 FF A7 08 01 00 1F F6 77 FF 20 09 40 FF A7 08 
    01 00 1F F6 77 FF 5A FF A7 92 22 65 A9 08 01 FF 13 63 A9 A9 46 FF 7F 91 
    A8 5B A9 5A A6 25 A7 95 96 FF A2 0C A3 95 A9 BD 12 0F 82 FE BE 82 BE 86 
    BE 8B BE 8E 06 00 00 9B 57 FF A8 08 7F FF 5A FF A6 93 F2 60 A8 28 00 80 
    AA 71 AB 92 ED 6F 20 FF 00 00 EA 6F 5A FF A4 93 A8 18 00 01 96 FF A8 5C 
    A9 A9 A8 08 7F FF A8 1C 00 80 A4 CB DD 6F 0E FE 4D 96 4C A8 4E 2B 4C 06 
    46 1E 05 8F 00 F8 4A A8 1F 76 A0 02 3A 06 4A 0F 6E 60 22 76 00 8F 44 01 
    A9 A8 3A 07 A9 8A C4 CC F8 FF 05 50 A9 88 00 8F 44 01 A9 A8 3A 07 A9 8A 
    C4 7E 01 3B 40 8F D0 07 2C FF FF FF 00 8F 36 01 42 1E A9 A8 3A 07 A9 8A 
    A9 A0 40 76 90 9F 00 52 03 61 00 9A 03 6F A9 28 00 02 4E 96 00 8F 44 01 
    1F 76 A0 02 A9 A8 3A 07 A9 8A C4 CC F8 FF 02 50 A9 88 00 8F 44 01 A9 A8 
    3A 07 A9 8A C4 7E 4D 92 30 52 03 61 06 52 03 61 4E 28 FF 01 40 76 FA A1 
    01 52 03 60 BF 56 4E 01 4E 92 2B 60 46 06 40 76 B1 96 4E 96 00 52 25 60 
    46 06 30 FF 46 1E 10 9A 40 76 12 97 06 9A 40 76 3E 9F 22 76 00 BE 1F 76 
    A0 02 88 02 3A 07 42 C2 A9 8A 46 06 40 76 90 9F 00 52 03 61 00 9A 03 6F 
    A9 28 00 02 4E 96 1A 76 00 52 07 60 06 9A 40 76 12 97 03 6F 4E 28 03 02 
    4E 92 8E FE 06 00 12 FE 4E A0 4C 1E 4A A8 51 2B 4A 06 48 1E 1F 76 A0 02 
    20 02 3A 07 A9 8A C4 06 50 1E 4C 06 42 1E 48 06 40 76 FD 9A 01 52 61 60 
    22 76 00 8F 80 01 1F 76 A0 02 A9 A8 3A 07 A9 8A C4 CC 02 00 C0 FF 52 96 
    00 02 00 8F 80 01 03 19 42 1E A9 A8 3A 07 A9 8A 02 02 40 76 90 9F 00 52 
    03 61 00 9A 03 6F A9 28 00 02 51 96 1F 76 A0 02 20 02 3A 07 A9 8A AB 28 
    FF FF AA 28 05 05 C4 A9 40 76 04 9F 51 92 12 60 56 06 42 1E 57 92 43 96 
    4A 8A 4E 83 4C 06 40 76 5A 95 51 96 00 52 06 61 4E 8A 00 02 F4 1E 51 28 
    F4 01 20 02 50 C4 1F 76 A0 02 3A 07 A9 8A C4 C2 01 29 00 02 00 8F 80 01 
    03 19 42 1E A9 A8 3A 07 A9 8A 03 56 52 01 00 9B 02 90 40 76 90 9F 00 52 
    05 61 51 92 03 60 00 9A 05 6F 51 92 03 60 A9 28 00 02 51 96 1A 76 03 6F 
    51 28 FA 01 51 92 92 FE 06 00 18 FE 4A A0 48 1E 46 A8 4F 2B 50 2B 4C 1E 
    5C 06 4E 1E 46 06 44 1E 44 06 40 76 BA 9D 4F 96 00 52 2B 60 46 06 52 1E 
    4C 06 A9 8A 81 DC 4C A8 60 61 4E 8A 52 83 C4 06 C5 0F 11 61 52 06 44 1E 
    4A 8A 44 06 C4 1E 52 8A 4A 83 C4 06 D5 1E 4E 8A 4A 83 C4 06 E5 1E 50 28 
    F4 01 4B 6F 5D 92 04 61 02 02 4E 07 4E 1E 02 02 52 07 52 1E 4C 06 A9 8A 
    81 DC 4C A8 DF 60 3D 6F 46 06 52 1E 5C 06 54 1E BF 56 55 02 4C 06 A9 8A 
    81 DC 4C A8 32 61 00 02 58 1E 55 0E 58 0F 20 69 58 06 54 07 A9 8A 58 06 
    C4 88 52 07 A9 8A C4 80 A6 06 A7 0F 0F 61 4A 8A 52 06 C4 1E 52 8A 4A 83 
    C4 0E D5 1E 54 8A 4A 83 C4 0E E5 1E 50 28 F4 01 07 6F 01 02 58 07 58 1E 
    55 0E 58 0F E2 66 5D 92 04 61 02 02 54 07 54 1E 02 02 52 07 52 1E 4C 06 
    A9 8A 81 DC 4C A8 D0 60 50 92 98 FE 06 00 02 FE 42 1E 40 76 DE A0 00 52 
    07 60 20 FF 28 03 00 8F DE A8 40 76 EB A2 04 02 48 0F 07 69 20 FF 29 03 
    00 8F DE A8 40 76 EB A2 46 06 07 60 20 FF 2A 03 00 8F DE A8 40 76 EB A2 
    4A 06 07 60 20 FF 2B 03 00 8F DE A8 40 76 EB A2 01 29 20 FF FF FF 48 0F 
    07 67 20 FF 2C 03 00 8F DE A8 40 76 EB A2 0F 8F FF FF A9 A8 46 0F 07 67 
    20 FF 2D 03 00 8F DE A8 40 76 EB A2 0F 8F FF FF A9 A8 4A 0F 07 67 20 FF 
    2E 03 00 8F DE A8 40 76 EB A2 22 76 46 88 08 02 42 07 A9 8A C4 7E 0A 02 
    42 07 A9 8A 46 A3 AA 18 0F 00 C4 CC F0 FF AA 98 0A 02 42 07 A9 8A C4 57 
    48 88 0C 02 42 07 A9 8A C4 7E 4A 88 10 02 42 07 A9 8A C4 7E 12 02 42 07 
    A9 8A 4A A3 AA 18 0F 00 C4 CC F0 FF AA 98 12 02 42 07 A9 8A C4 57 1A 76 
    82 FE 06 00 08 FE 47 7C 42 1E E0 02 42 0F 13 66 FD 02 42 0F 10 68 EA 02 
    42 0F 0D 61 EB 02 42 0F 0A 61 F3 02 42 0F 07 61 F6 02 42 0F 04 61 FA 02 
    42 0F 0D 60 14 02 42 0F 0A 61 15 02 42 0F 07 61 20 FF AB 01 00 8F C4 A9 
    40 76 EB A2 01 02 A6 1E 42 92 1F 90 A9 2D A6 06 3B 56 46 1E 01 29 42 06 
    44 FF 34 FF 30 FF 1A FF 1F 00 44 1E 22 76 47 92 01 52 18 60 14 02 44 07 
    A9 8A 46 06 C4 98 CC 99 14 02 42 0F 04 61 15 02 42 0F 24 60 42 06 05 8F 
    02 D8 44 FF 30 FF 01 56 A4 00 46 06 C4 98 CC 99 19 6F 14 02 44 07 A9 8A 
    46 06 55 FF C4 C0 CC C1 14 02 42 0F 04 61 15 02 42 0F 0C 60 42 06 05 8F 
    02 D8 44 FF 30 FF 01 56 A4 00 46 06 55 FF C4 C0 CC C1 1A 76 88 FE 06 00 
    06 FE 44 1E 45 2B 22 76 08 8F 00 00 A9 A8 44 0F 19 66 09 8F 00 00 A9 A8 
    44 0F 14 69 00 02 1F 76 A0 02 08 19 42 1E 28 02 3A 07 A9 8A 00 02 40 76 
    90 9F 00 52 03 61 00 9A 03 6F A9 28 00 02 45 96 3D 6F 09 8F 00 00 A9 A8 
    44 0F 19 66 0A 8F 00 00 A9 A8 44 0F 14 69 00 02 1F 76 A0 02 08 19 42 1E 
    28 02 3A 07 A9 8A 01 02 40 76 90 9F 00 52 03 61 00 9A 03 6F A9 28 00 02 
    45 96 20 6F 0A 8F 00 00 A9 A8 44 0F 19 66 0B 8F 00 00 A9 A8 44 0F 14 69 
    00 02 1F 76 A0 02 08 19 42 1E 28 02 3A 07 A9 8A 02 02 40 76 90 9F 00 52 
    03 61 00 9A 03 6F A9 28 00 02 45 96 03 6F 45 28 FA 01 1A 76 45 92 86 FE 
    06 00 02 FE 41 96 42 96 10 52 0D 61 18 52 0B 61 16 52 09 61 14 52 07 61 
    02 52 05 61 08 52 03 61 06 52 43 60 22 76 00 8F 44 01 1F 76 A0 02 A9 A8 
    3A 07 A9 8A C4 CC F8 FF 05 50 A9 88 00 8F 44 01 A9 A8 3A 07 A9 8A C4 7E 
    00 8F 06 01 A9 A8 3A 07 A9 8A 42 92 3F 90 A9 88 C4 CD C0 FF A6 99 00 8F 
    06 01 A9 A8 3A 07 A9 8A C4 7E 00 8F 5A 01 A9 A8 3A 07 A9 8A C4 CC E0 FF 
    15 50 A9 88 00 8F 5A 01 A9 A8 3A 07 A9 8A C4 7E 00 8F 44 01 A9 A8 3A 07 
    A9 8A C4 CC F8 FF 02 50 A9 88 00 8F 44 01 A9 A8 3A 07 A9 8A C4 7E 1A 76 
    00 9A 82 FE 06 00 06 FE 42 1E 40 76 30 A1 00 52 06 60 00 8F C4 A9 B4 02 
    40 76 EB A2 42 06 01 29 44 FF 34 FF 30 FF 1A FF 1F 00 44 1E 01 02 A6 1E 
    42 92 1F 90 A9 2D A6 06 3B 56 46 1E 22 76 4A 06 A9 42 08 6C 12 02 44 07 
    A9 8A 46 06 C4 98 CC 99 08 6F 12 02 44 07 A9 8A 46 06 55 FF C4 C0 CC C1 
    4A 06 A9 40 09 6C 0C 02 44 07 A9 8A 46 06 55 FF C4 C0 CC C1 07 6F 0C 02 
    44 07 A9 8A 46 06 C4 98 CC 99 4A 06 A9 41 08 6C 10 02 44 07 A9 8A 46 06 
    C4 98 CC 99 08 6F 10 02 44 07 A9 8A 46 06 55 FF C4 C0 CC C1 1A 76 86 FE 
    06 00 02 FE 41 2B 42 2B 22 76 05 8F 3A D2 C4 1A 07 00 05 F6 00 77 05 8F 
    32 D2 C4 18 FE FF 2D F6 00 77 C4 18 FD FF 2D F6 00 77 1A 76 69 FF 40 76 
    B8 99 41 96 22 76 05 8F 08 D2 C4 CC FC FF 01 50 C4 96 FA F6 00 77 32 F6 
    00 77 1A 76 0F 6F 40 76 E4 A2 40 76 B8 99 41 96 22 76 05 8F 08 D2 C4 CC 
    FC FF 01 50 C4 96 1A 76 42 0A 69 FF 40 76 96 A2 00 52 06 61 41 92 04 60 
    42 92 04 52 E9 68 41 92 04 60 25 76 00 52 FE 61 82 FE 69 FF 06 00 
    00 08 00 00 00 98 02 FE 42 1E 02 8F 00 00 A9 A8 42 0F 13 61 42 06 11 61 
    01 8F 00 00 A9 A8 42 0F 0C 61 03 8F 00 00 A9 A8 42 0F 07 61 20 FF 91 02 
    00 8F 2A A9 40 76 EB A2 22 76 1D 6F 05 8F 08 D2 C4 18 F7 FF FA F6 00 77 
    32 F6 00 77 C4 18 FC FF 24 6F 40 76 BA 97 21 6F 40 76 71 9D 1E 6F 05 8F 
    08 D2 C4 CC FC FF 02 50 C4 96 FA F6 00 77 32 F6 00 77 13 6F 42 C4 A6 06 
    E2 61 01 8F 00 00 A9 A8 A6 0F E8 61 02 8F 00 00 A9 A8 A6 0F E9 61 03 8F 
    00 00 A9 A8 A6 0F E1 61 1A 76 82 FE 69 FF 06 00 0A FE 42 A8 07 8F 20 80 
    46 A8 0D 02 48 1E 00 02 4A 1E 05 8F 00 F0 C4 06 44 1E AC 28 12 00 3B 56 
    44 1E 15 6F 44 06 00 90 A8 18 00 80 58 FF 09 60 01 02 4A 1E 48 06 34 FF 
    16 FF 01 1E 46 1E 07 6F 01 02 41 56 48 00 44 06 30 FF 44 1E 4A 06 03 60 
    48 06 E9 63 46 8A C4 06 44 1E 46 8A D4 06 44 1E E4 06 44 1E F4 06 44 1E 
    42 06 15 61 42 8A C4 06 05 8F 10 F0 C4 1E 42 8A D4 06 05 8F 12 F0 C4 1E 
    42 8A E4 06 05 8F 14 F0 C4 1E 42 8A F4 06 05 8F 16 F0 C4 1E 8A FE 06 00 
    0A FE 42 A8 07 8F 20 82 46 A8 0D 02 48 1E 00 02 4A 1E 05 8F 80 F0 C4 06 
    44 1E AC 28 12 00 3B 56 44 1E 15 6F 44 06 00 90 A8 18 00 80 58 FF 09 60 
    01 02 4A 1E 48 06 34 FF 16 FF 09 1E 46 1E 07 6F 01 02 41 56 48 00 44 06 
    30 FF 44 1E 4A 06 03 60 48 06 E9 63 46 8A C4 06 44 1E 46 8A D4 06 44 1E 
    E4 06 44 1E F4 06 44 1E 42 06 15 61 42 8A C4 06 05 8F 90 F0 C4 1E 42 8A 
    D4 06 05 8F 92 F0 C4 1E 42 8A E4 06 05 8F 94 F0 C4 1E 42 8A F4 06 05 8F 
    96 F0 C4 1E 8A FE 06 00 08 FE 46 97 45 96 44 A0 42 A8 40 76 F2 A2 24 8F 
    FE 9E A9 A8 40 76 58 02 A9 28 E4 1B 40 76 4B 9D 4B 92 40 76 4B 9D 1F 76 
    A0 02 30 2B 45 92 40 76 4B 9D 46 92 40 76 4B 9D 47 2B 47 92 02 52 0C 63 
    01 3B 47 85 42 07 A9 8A C4 92 40 76 4B 9D 47 0A 47 92 02 52 F6 64 4C 92 
    40 76 4B 9D 47 2B 47 92 02 52 0C 63 01 3B 47 85 44 07 A9 8A C4 92 40 76 
    4B 9D 47 0A 47 92 02 52 F6 64 40 76 5A 9F A9 28 1B E4 40 76 4B 9D 40 76 
    72 A2 88 FE 06 00 02 FE 41 96 A9 28 FC 01 41 54 06 60 1F 76 A0 02 36 28 
    00 70 3B 6F A9 28 FD 01 41 54 06 60 1F 76 A0 02 36 28 00 80 32 6F A9 28 
    FE 01 41 54 06 60 1F 76 A0 02 36 28 00 90 29 6F A9 28 00 02 41 54 06 60 
    1F 76 A0 02 36 28 00 A0 20 6F A9 28 FF 01 41 54 06 60 1F 76 A0 02 36 28 
    00 B0 17 6F A9 28 FA 01 41 54 06 60 1F 76 A0 02 36 28 00 C0 0E 6F A9 28 
    F4 01 41 54 06 60 1F 76 A0 02 36 28 00 E0 05 6F 1F 76 A0 02 32 28 00 F0 
    82 FE 06 00 02 FE 42 1E 40 76 57 A1 00 52 07 60 20 FF 09 01 00 8F 5C AA 
    40 76 EB A2 01 BE 46 06 00 9B 01 90 A6 0F 06 60 01 02 42 07 A9 8A C4 18 
    BF FF 02 BE 46 06 00 9B 02 90 A6 0F 06 60 04 02 42 07 A9 8A C4 18 FD FF 
    04 BE 46 06 00 9B 04 90 A6 0F 06 60 04 02 42 07 A9 8A C4 18 FE FF 08 BE 
    46 06 00 9B 08 90 A6 0F 06 60 0A 02 42 07 A9 8A C4 18 DF FF 10 BE 46 06 
    00 9B 10 90 A6 0F 06 60 0B 02 42 07 A9 8A C4 18 DF FF 82 FE 06 00 04 FE 
    43 2B 00 02 42 1E 44 2B 20 FF D0 07 40 76 58 02 45 8F 30 D2 20 FF FF 01 
    C5 0F 0A 67 05 8F 30 D2 C4 06 01 51 C4 1E 20 FF FF 01 C5 0F FA 68 05 8F 
    30 D2 A9 28 FF 07 C4 54 14 61 01 02 42 07 42 1E 26 8F A0 25 A9 A8 42 0F 
    06 67 43 92 03 52 09 60 44 2B 07 6F 05 8F 30 D2 A9 28 FF 07 C4 54 EE 60 
    43 92 03 52 09 60 05 8F 30 D2 A9 28 FF 07 C4 54 03 60 BF 56 44 01 43 0A 
    00 02 42 1E 43 92 04 52 CA 68 44 92 84 FE 06 00 08 FE 44 A0 42 A8 40 76 
    C3 9F A9 88 20 FF E4 1B A6 0F 05 61 40 76 CE A2 64 9A 35 6F 40 76 C3 9F 
    42 8A C4 96 30 2B 40 76 C3 9F 45 96 46 2B 46 2B 01 3B 09 6F 40 76 C3 9F 
    A9 88 46 85 44 07 A9 8A C4 7E 46 0A 42 8A C4 92 C0 FF 46 54 F4 66 30 92 
    47 96 40 76 C3 9F 47 88 A9 0E A6 0F 05 61 40 76 CE A2 65 9A 10 6F 40 76 
    C3 9F A9 88 01 29 20 FF 1B E4 A6 0F 05 61 40 76 CE A2 66 9A 04 6F 40 76 
    C6 A2 45 92 88 FE 06 00 06 FE 42 1E 1F 76 A0 02 32 28 00 10 A9 28 78 65 
    A8 28 34 12 34 1E 36 28 00 10 00 02 38 1E 00 8F DC 9F 1F 76 A1 02 00 A8 
    40 76 DC 9F A9 88 20 FF AA 08 A6 0F 0C 61 1F 76 A0 02 32 28 00 30 08 8F 
    00 00 34 A8 36 28 00 10 00 02 38 1E 40 76 CC A1 40 76 6A A1 44 1E 40 76 
    68 8A 45 2B 45 2B 45 1B A4 7F 05 67 45 0A 45 1B A4 7F FD 68 45 2B 45 1B 
    A4 7F 05 67 45 0A 45 1B A4 7F FD 68 44 06 86 FE 06 00 04 FE 42 1E 40 76 
    57 A1 00 52 06 60 00 8F 5C AA 39 02 40 76 EB A2 4A 06 06 60 00 8F 5C AA 
    3A 02 40 76 EB A2 4A 06 33 FF 48 0F 06 69 00 8F 5C AA 3B 02 40 76 EB A2 
    42 06 40 76 00 A0 4A 06 32 FF A6 1E 48 A3 00 02 1F F6 17 56 A6 00 A9 A9 
    01 19 44 1E 01 29 42 8A A9 18 00 FF 00 91 47 FF D4 96 42 8A 44 92 FF 90 
    DC 96 42 8A C4 CC 18 FF 4C CA C4 96 42 06 40 76 44 A1 84 FE 06 00 40 76 
    31 A2 26 76 00 00 2F 76 00 00 00 9A A9 F4 E2 0C A9 F4 E4 0C A9 F4 E6 0C 
    A9 F4 E8 0C A9 F4 EA 0C A9 F4 EC 0C A9 F4 EE 0C A9 F4 F0 0C A9 F4 F2 0C 
    A9 F4 F4 0C A9 F4 F6 0C A9 F4 F8 0C A9 F4 E3 0C A9 F4 E5 0C A9 F4 E7 0C 
    A9 F4 E9 0C A9 F4 EB 0C A9 F4 ED 0C A9 F4 EF 0C A9 F4 F1 0C A9 F4 F3 0C 
    A9 F4 F5 0C A9 F4 F7 0C A9 F4 F9 0C A9 F5 E0 0C 01 50 A9 F4 E0 0C 06 00 
    04 FE 42 1E 07 8F 00 80 A9 A8 42 0F 08 66 48 06 07 8F 00 8C 30 FF 42 07 
    A4 0F 27 69 08 8F 00 00 A9 A8 42 0F 08 66 48 06 0B 8F 00 00 30 FF 42 07 
    A4 0F 1B 69 2F FF 10 02 42 0F 0A 66 48 06 AB 28 00 60 AA 28 08 01 30 FF 
    42 07 AB 0F 0E 69 2C FF 71 10 42 0F 0D 66 48 06 AB 28 80 11 AA 28 07 01 
    30 FF 42 07 AB 0F 04 66 BF 56 43 01 02 6F 43 2B 43 92 84 FE 06 00 08 FE 
    47 96 48 2B 40 76 FA A1 02 52 2C 60 05 8F 00 F8 46 A8 1F 76 A0 02 3A 06 
    46 0F 21 60 47 92 02 52 1B 66 22 76 00 02 08 19 42 1E 47 88 28 02 3A 07 
    A9 8A A6 06 40 76 90 9F 00 52 03 61 00 9A 03 6F A9 28 F9 01 48 96 00 52 
    05 60 00 9A 40 76 C3 83 48 96 1A 76 09 6F 48 28 F9 01 06 6F 48 28 03 02 
    03 6F BF 56 48 01 48 92 88 FE 06 00 08 FE 42 1E A8 0E 1A FF 1F 00 44 1E 
    01 29 42 06 47 FF 00 9B FF 90 48 1E 48 2D 03 02 3B 56 46 1E 22 76 44 8A 
    55 FF C4 C0 CC C1 1A 02 44 07 A9 8A 48 2D 46 06 55 FF C4 CE CC CF A6 1E 
    42 06 41 FF 00 9B 03 90 3B 56 5A FF A6 06 AB CA AA CB A6 1E 1A 02 44 07 
    A9 8A C4 C2 48 2D 42 06 44 8A 00 9B 03 90 3B 56 C4 98 CC 99 1A 76 88 FE 
    06 00 0A FE 49 7C 42 1E 40 76 30 A1 00 52 07 60 20 FF 24 01 00 8F C4 A9 
    40 76 EB A2 42 06 01 29 44 FF 34 FF 30 FF 1A FF 1F 00 44 1E 42 06 00 9B 
    0F 90 30 FF 48 1E 42 06 00 9B 1F 90 43 FF 01 09 46 1E 22 76 48 2D 46 06 
    30 FF 44 07 A9 8A 03 02 3B 56 55 FF C4 C0 CC C1 46 06 30 FF 44 07 A9 8A 
    48 2D 49 0E 3B 56 C4 98 CC 99 1A 76 8A FE 06 00 0C FE 48 1E 46 A8 4B 2B 
    46 06 4A 1E 05 8F 00 F8 44 A8 44 06 4A 0F 04 61 4A A8 4B 28 04 02 48 92 
    1F 76 A0 02 3F 96 4A 06 3A 1E 4A 8A C4 CC 00 0F C7 FF 3E 96 00 8F 00 02 
    A9 A8 4A 07 A9 8A C4 92 C3 FF A9 CC C0 01 C2 FF 3C 96 00 8F 00 02 A9 A8 
    4A 07 A9 8A C4 CC 80 03 C3 FF C2 FF 3D 96 4B 92 8C FE 06 00 22 76 1A 02 
    1F 76 A0 02 3A 07 A9 8A 40 8F FF FF C4 A0 00 8F 44 01 A9 A8 3A 07 A9 8A 
    C4 CC F8 FF 05 50 A9 88 00 8F 44 01 A9 A8 3A 07 A9 8A 00 B6 C4 7E 00 8F 
    52 01 A9 A8 3A 07 A9 8A C4 C3 00 8F 44 01 A9 A8 3A 07 A9 8A C4 CC F8 FF 
    02 50 A9 88 00 8F 44 01 A9 A8 3A 07 A9 8A C4 7E 1A 76 00 9A 06 00 08 FE 
    47 7C 42 1E 40 76 30 A1 00 52 06 60 00 8F C4 A9 3A 02 40 76 EB A2 42 06 
    01 29 44 FF 34 FF 30 FF 1A FF 1F 00 44 1E 01 02 A6 1E 42 92 1F 90 A9 2D 
    A6 06 3B 56 46 1E 22 76 47 92 01 52 08 60 0A 02 44 07 A9 8A 46 06 C4 98 
    CC 99 08 6F 0A 02 44 07 A9 8A 46 06 55 FF C4 C0 CC C1 1A 76 88 FE 06 00 
    84 2F AB 2B 18 6F A9 A0 A0 01 01 19 A7 1E 81 DE 87 58 00 02 81 DE 01 19 
    85 78 A6 0F FA 60 03 6F 84 92 85 96 AA 92 C0 FF A9 2F AB 92 01 9C A9 27 
    10 52 E7 63 AA 40 F5 6D 84 92 A9 CD 0F 00 02 9D C3 FF A8 88 A9 58 11 53 
    04 60 A6 06 84 0D A6 1E A0 80 20 FF FF 0F A7 0F D7 60 06 00 08 FE 47 96 
    42 A8 00 8F FF FF 44 A8 46 A8 48 2B 48 54 1D 69 42 8A 48 92 01 F0 A9 58 
    94 0E 44 07 44 1E 44 A3 AA 18 00 00 A8 0E 01 56 AB 00 44 A9 44 06 46 07 
    46 1E 46 A3 A8 0E AA 18 00 00 01 56 AB 00 46 A9 48 0A 47 92 48 54 E5 66 
    46 06 3F FF 44 CA 43 CB 88 FE 06 00 08 FE 42 1E 00 02 44 1E 42 06 46 1E 
    BF 56 47 01 47 92 20 52 1A 66 AC 28 1F 00 46 06 22 56 5A FF 44 06 30 FF 
    AB CA AA CB 44 1E 46 06 30 FF 46 1E 4C 06 44 0F 06 66 41 56 44 00 01 02 
    46 07 46 1E 47 0A 47 92 20 52 EA 69 44 06 04 61 4E 06 46 07 46 1E 46 06 
    88 FE 06 00 08 FE 48 1E 22 76 07 9A 40 76 58 A2 20 FF 00 72 40 76 16 A2 
    A9 28 80 C3 A8 28 C9 01 07 BE 00 8F 80 25 42 1E 44 A8 20 FF 00 72 46 C2 
    40 76 82 9A 20 FF 00 72 40 76 B5 A2 07 02 42 1E 20 FF 00 72 40 76 73 99 
    20 FF 00 72 40 76 08 A2 1A 76 48 06 40 76 CC 91 88 FE 06 00 02 FE 42 1E 
    42 8A D4 2B 42 8A BF 56 DC 01 0C 02 42 07 A9 8A C4 1A 00 20 0C 02 42 07 
    A9 8A C4 1A 00 40 01 29 0C 02 42 07 A9 83 C5 CC 00 80 A9 88 20 FF 00 80 
    A6 0F F7 60 0C 02 42 07 A9 8A C4 1A 00 40 0C 02 42 07 A9 8A C4 18 FF DF 
    82 FE 06 00 02 FE 41 96 41 CC FF 00 A9 5C 20 FF 00 72 40 76 EB A1 1F 76 
    A0 02 41 92 FF 90 30 72 40 76 F2 A2 40 76 72 A2 41 CC 00 FF C7 FF A9 5C 
    20 FF 00 72 40 76 EB A1 1F 76 A0 02 41 CC 00 FF C7 FF 30 72 40 76 F2 A2 
    40 76 72 A2 82 FE 06 00 02 FE 41 2B 22 76 05 8F 32 D2 C4 18 FE FF 2D F6 
    00 77 C4 1A 02 00 2D F6 00 77 1A 76 69 FF 40 76 B8 99 41 96 22 76 05 8F 
    08 D2 C4 CC FC FF 01 50 C4 96 1A 76 69 FF 02 6F 25 76 40 76 96 A2 00 52 
    03 61 41 92 FA 61 82 FE 06 00 04 FE 43 7C 42 1E 40 76 DE A0 00 52 07 60 
    20 FF 90 01 00 8F DE A8 40 76 EB A2 A9 28 00 0A 43 54 0A 60 22 76 42 8A 
    C4 CC FF F0 A9 1A 00 0A C4 96 1A 76 09 6F 22 76 42 8A C4 CC FF F0 A9 1A 
    00 0B C4 96 1A 76 84 FE 06 00 04 FE 42 1E 43 2B 2F FF 10 02 42 0F 05 66 
    2D FF 43 08 42 0F 15 66 2F FF 0E 02 42 0F 07 66 A9 28 80 01 A8 28 07 01 
    42 0F 0B 66 2C FF 71 10 42 0F 09 66 A9 28 80 11 A8 28 07 01 42 0F 03 69 
    BF 56 43 01 43 92 84 FE 06 00 04 FE 05 8F 18 F0 C4 06 42 1E 41 46 06 6C 
    41 45 04 6C BF 56 43 01 15 6F 00 90 10 91 10 8F 00 00 A4 0F 04 60 BF 56 
    43 03 0C 6F 42 06 08 8F 00 00 00 90 08 91 A4 0F 04 60 BF 56 43 02 02 6F 
    43 2B 43 92 84 FE 06 00 04 FE 05 8F 98 F0 C4 06 42 1E 41 46 06 6C 41 45 
    04 6C BF 56 43 01 15 6F 00 90 10 91 10 8F 00 00 A4 0F 04 60 BF 56 43 03 
    0C 6F 42 06 08 8F 00 00 00 90 08 91 A4 0F 04 60 BF 56 43 02 02 6F 43 2B 
    43 92 84 FE 06 00 02 FE 42 1E 40 76 89 A0 00 52 10 61 0A 02 42 07 A9 8A 
    00 9A C4 CD 00 1F 00 53 03 61 01 9B 02 6F 00 9B 00 53 0F 61 01 9A 0D 6F 
    42 8A 00 9A E4 93 40 91 40 53 03 60 00 9B 02 6F 01 9B 00 53 02 61 01 9A 
    82 FE 06 00 04 FE 40 76 F2 A2 40 76 76 9F 40 76 7C A1 10 3B 69 FF 40 76 
    C0 9A 40 76 E6 9E 26 76 00 00 2F 76 00 00 05 8F 00 FB 45 8F 00 F8 42 A8 
    A9 A0 05 D4 40 76 28 01 40 76 46 A0 01 02 40 76 3E 87 44 1E 84 FE 06 00 
    1F 56 22 76 C0 B9 29 28 68 00 1A 76 40 76 47 9E 01 6F AD 28 00 04 BD 2B 
    BD 2B BD 1E 07 00 33 56 AC 1E A9 58 A9 59 A9 5A A9 5B A9 5C A9 5D A9 88 
    A9 80 1F 76 00 00 BD 2B BD 28 0B 0A 00 76 13 76 06 00 02 FE 41 96 42 2B 
    40 76 FA A1 01 52 03 60 BF 56 42 01 42 92 13 60 41 92 10 52 07 61 18 52 
    05 61 16 52 03 61 14 52 08 60 10 9A 40 76 12 97 41 92 40 76 12 97 03 6F 
    42 28 FF 01 42 92 82 FE 06 00 04 FE 43 7C 42 1E 40 76 DE A0 00 52 07 60 
    20 FF C5 02 00 8F DE A8 40 76 EB A2 22 76 28 02 42 07 A9 8A C4 CC E0 0F 
    43 CA A9 88 A6 1A 00 A0 28 02 42 07 A9 8A C4 7E 1A 76 84 FE 06 00 04 FE 
    43 7C 42 1E 40 76 DE A0 00 52 07 60 20 FF A1 02 00 8F DE A8 40 76 EB A2 
    22 76 24 02 42 07 A9 8A C4 CC E0 0F 43 CA A9 88 A6 1A 00 A0 24 02 42 07 
    A9 8A C4 7E 1A 76 84 FE 06 00 02 FE 22 76 BF 56 41 03 41 92 E0 52 0D 67 
    00 8F 73 A0 03 56 41 01 A9 08 00 0D A9 5D C5 A8 41 0A 41 92 E0 52 F7 68 
    00 8F AB A2 A4 BD 24 0D 00 8F A1 A2 A4 BD 26 0D 1A 76 82 FE 06 00 06 FE 
    00 02 46 1E 08 8F 00 20 44 A8 44 8A C4 06 46 1E 08 8F 00 21 44 A8 44 8A 
    C4 06 46 1E 08 8F 00 22 44 A8 44 8A C4 06 46 1E 08 8F 00 23 44 A8 44 8A 
    C4 06 46 1E 86 FE 06 00 00 52 AB A8 A4 C5 07 61 A9 88 81 DE 85 5C 87 7C 
    0E 00 FE FF A9 88 A6 0F 0F 61 00 53 0D 61 FF 9D A8 5C BF 76 FE FF 85 92 
    87 96 0E 00 FE FF 85 92 87 96 0C 00 F8 FF A4 A9 06 00 02 FE 41 96 02 52 
    03 61 06 52 14 60 22 76 18 02 1F 76 A0 02 3A 07 A9 8A C4 1A 01 00 40 76 
    0F 9C 22 76 1F 76 A0 02 18 02 3A 07 A9 8A C4 18 FE FF 1A 76 00 9A 82 FE 
    06 00 1F 76 A0 02 30 CC FF 00 A9 5C 20 FF 00 72 40 76 EB A1 40 76 F2 A2 
    40 76 72 A2 1F 76 A0 02 30 CC 00 FF C7 FF A9 5C 20 FF 00 72 40 76 EB A1 
    40 76 F2 A2 40 76 72 A2 06 00 40 76 8B A2 A8 28 85 81 A9 28 30 01 40 76 
    61 8E 02 9A 40 76 4B A2 40 76 05 A3 40 76 FE 90 40 76 D6 A2 00 D4 14 02 
    40 76 47 96 00 D4 15 02 40 76 47 96 06 00 08 FE 48 1E 46 A8 C4 06 44 1E 
    4C 06 44 CE 43 CF 48 CA 47 CB 44 1E C4 1E 46 8A 00 BE C4 06 44 0F 03 60 
    01 9B 02 6F 00 9B 00 53 02 61 01 BE A6 92 88 FE 06 00 02 FE 41 96 22 76 
    01 52 07 60 05 8F 22 D2 C4 2B 2D F6 00 77 0B 6F 41 93 01 90 05 8F 22 D2 
    D0 FF 87 FF A8 CA C4 96 2D F6 00 77 1A 76 82 FE 69 FF 06 00 02 FE 41 2B 
    42 2B 20 FF 00 72 40 76 7F A2 41 96 20 FF 00 72 40 76 7F A2 42 96 1F 76 
    A0 02 41 92 30 94 42 94 30 96 03 56 42 08 41 98 41 92 82 FE 06 00 02 FE 
    41 2B 42 2B 20 FF 00 72 40 76 7F A2 41 96 20 FF 00 72 40 76 7F A2 42 96 
    1F 76 A0 02 41 92 30 94 42 94 30 96 03 56 42 08 41 98 41 92 82 FE 06 00 
    04 FE 42 1E 48 87 01 29 44 56 42 00 45 FF 44 1E 22 76 84 FE 06 00 
    09 03 00 00 00 A0 02 FE 42 1E 40 76 57 A1 00 52 07 60 20 FF 21 02 00 8F 
    10 AA 40 76 EB A2 0A 02 42 07 A9 8A C4 18 FF BF 01 02 42 07 A9 8A C4 18 
    FC FF 82 FE 06 00 04 FE 41 96 1F 90 80 FF 42 96 41 CC 00 1F C7 FF 43 96 
    22 76 05 8F 22 D3 A9 A8 42 0D A9 8A 43 2D 01 02 3B 56 C4 98 CC 99 1A 76 
    84 FE 06 00 04 FE 41 96 1F 90 80 FF 42 96 41 CC 00 1F C7 FF 43 96 22 76 
    05 8F 22 D3 A9 A8 42 0D A9 8A 43 2D 01 02 3B 56 C4 98 CC 99 1A 76 84 FE 
    06 00 02 FE 22 76 05 8F 00 F8 78 02 40 76 DD 9B 41 96 00 52 03 61 40 76 
    52 02 00 9A 40 76 38 9B 41 96 00 52 03 61 40 76 52 02 1A 76 82 FE 06 00 
    02 FE 42 1E 40 76 DE A0 00 52 07 60 20 FF 6B 01 00 8F DE A8 40 76 EB A2 
    22 76 42 8A C4 CC FF 0F A9 1A 00 50 C4 96 1A 76 82 FE 06 00 1B 76 F0 FF 
    00 E2 BD 00 30 E6 00 06 02 FE 42 29 16 56 41 F5 E0 0C 41 92 FE 90 C0 FF 
    42 96 41 1B 00 0E 03 68 42 08 80 00 25 76 00 6F 02 FE 42 1E 0A 02 42 07 
    A9 83 C5 CC 00 40 A9 80 00 BE 20 FF 00 40 A7 0F 03 60 01 9B 02 6F 00 9B 
    00 53 02 61 01 BE A6 92 82 FE 06 00 02 FE 42 1E 40 76 DE A0 00 52 07 60 
    20 FF 2E 02 00 8F DE A8 40 76 EB A2 22 76 14 02 42 07 A9 8A C4 1A 02 00 
    1A 76 82 FE 06 00 02 FE 42 1E 40 76 DE A0 00 52 07 60 20 FF 11 02 00 8F 
    DE A8 40 76 EB A2 22 76 14 02 42 07 A9 8A C4 1A 01 00 1A 76 82 FE 06 00 
    02 FE 42 1E 40 76 DE A0 00 52 07 60 20 FF 4C 01 00 8F DE A8 40 76 EB A2 
    22 76 42 8A C4 CC 0F FF 50 50 C4 96 1A 76 82 FE 06 00 02 FE 42 1E 05 8F 
    00 E7 00 BE 01 B6 A9 A8 42 0F 07 61 05 8F 40 E7 A9 A8 42 0F 02 61 00 B6 
    A7 93 02 61 01 BE A6 92 82 FE 06 00 06 FE 45 7C 42 1E 01 29 03 56 45 05 
    30 FF 1A FF 1F 00 44 1E 22 76 3C 02 44 07 A9 8A 42 06 55 FF C4 C0 CC C1 
    1A 76 86 FE 06 00 02 FE 42 1E 40 76 DE A0 00 52 06 60 00 8F DE A8 F0 02 
    40 76 EB A2 22 76 42 8A C4 CC F0 FF 05 50 C4 96 1A 76 82 FE 06 00 02 FE 
    42 1E 40 76 DE A0 00 52 06 60 00 8F DE A8 D2 02 40 76 EB A2 22 76 42 8A 
    C4 CC F0 FF 0A 50 C4 96 1A 76 82 FE 06 00 02 FE 42 1E 3D 02 00 BE 01 B6 
    42 0F 08 67 E0 02 42 0F 04 66 FD 02 42 0F 02 67 00 B6 A7 93 02 61 01 BE 
    A6 92 82 FE 06 00 02 FE 42 1E 40 76 57 A1 00 52 07 60 20 FF 06 02 00 8F 
    10 AA 40 76 EB A2 01 02 42 07 A9 8A C4 1A 23 00 82 FE 06 00 02 FE 42 1E 
    20 FF 00 72 00 BE 01 B6 42 0F 06 61 20 FF 10 72 42 0F 02 61 00 B6 A7 93 
    02 61 01 BE A6 92 82 FE 06 00 02 FE 1F 76 A1 02 00 C5 67 3E 01 29 A9 25 
    42 1E 1F 76 A1 02 00 C5 67 3E A9 0E 42 98 41 99 42 06 82 FE 06 00 00 02 
    00 D4 01 19 40 76 F3 A0 00 02 01 D4 01 19 40 76 F3 A0 00 02 07 D4 01 19 
    40 76 F3 A0 06 00 02 FE 42 1E 05 8F 00 F8 00 BE 00 B6 A9 A8 42 0F 02 60 
    01 B6 A7 93 02 61 01 BE A6 92 82 FE 06 00 02 FE 42 1E 05 8F 00 FB 00 BE 
    00 B6 A9 A8 42 0F 02 60 01 B6 A7 93 02 61 01 BE A6 92 82 FE 06 00 02 FE 
    42 1E 42 8A 00 9A EC 93 40 91 40 53 03 60 01 9B 02 6F 00 9B 00 53 02 61 
    01 9A 82 FE 06 00 02 FE 42 1E 42 8A 00 9A E4 93 80 91 80 53 03 60 01 9B 
    02 6F 00 9B 00 53 02 61 01 9A 82 FE 06 00 02 FE BF 56 41 01 41 92 08 52 
    09 66 1F 76 A1 02 00 C5 67 3E 41 0A 41 92 08 52 F9 69 82 FE 06 00 0A FE 
    4A A0 48 1E 46 A8 4A 06 42 1E BF 56 43 02 4E 83 46 8A 48 06 40 76 E0 94 
    8A FE 06 00 04 FE 43 7C 42 1E 42 06 40 76 BC A1 00 52 FC 61 43 88 09 02 
    42 07 A9 8A C4 7E 84 FE 06 00 2A 02 1F 76 A0 02 3A 07 A9 8A C4 CC 00 01 
    C7 FF 01 52 03 60 01 9A 02 6F 02 9A 06 00 02 FE 42 1E 01 02 42 07 A9 8A 
    C4 18 DF FF 01 02 42 07 A9 8A C4 1A 20 00 82 FE 06 00 02 FE 42 1E 0A 02 
    42 07 A9 8A C4 18 FF 7F 0A 02 42 07 A9 8A C4 1A 00 80 82 FE 06 00 08 FE 
    48 1E 46 A8 4C 06 44 1E 48 06 46 07 A9 8A 44 92 40 76 9F 9C 88 FE 06 00 
    00 9A 08 76 30 3B BE 93 A8 40 03 6C 01 9B 02 6F 00 9B 00 53 02 61 01 9A 
    06 00 22 76 A9 F5 29 70 A9 CC BF FF 28 50 A9 F4 29 70 2D F6 00 77 1A 76 
    69 FF 06 00 02 FE 41 96 22 76 05 8F 2C D2 C4 06 A9 18 F8 FF 41 AF C4 1E 
    1A 76 82 FE 06 00 02 FE 41 96 22 76 05 8F 2C D2 C4 06 A9 18 F8 FF 41 AF 
    C4 1E 1A 76 82 FE 06 00 CC 8A 00 02 01 19 81 DC A4 0F 07 61 00 02 81 DC 
    85 2B 01 19 A4 0F FB 60 06 00 02 FE 20 FF 00 72 40 76 7F A2 41 96 2D 52 
    03 61 01 9A 02 6F 00 9A 82 FE 06 00 02 FE 42 1E 42 06 40 76 AC A1 00 52 
    FC 61 42 8A FC CC FF 00 82 FE 06 00 22 76 A9 F5 29 70 68 50 A9 F4 29 70 
    2D F6 00 77 1A 76 69 FF 06 00 20 FF 00 00 05 8F 2E D2 C4 40 02 6C 01 9B 
    00 53 02 61 01 9A 06 00 1B 76 F0 FF 00 E2 BD 00 30 E6 00 06 42 29 16 56 
    25 76 00 6F 1B 76 F0 FF 00 E2 BD 00 30 E6 00 06 42 29 16 56 25 76 00 6F 
    02 FE 42 1E 01 02 42 07 A9 8A C4 1A 23 00 82 FE 06 00 A5 C4 A4 83 CD 06 
    A6 8A 03 DD 40 76 21 9F 06 00 20 FF 00 72 2D D4 40 76 EB A1 40 76 F2 A2 
    06 00 20 FF 00 72 A5 D4 40 76 EB A1 40 76 F2 A2 06 00 22 76 05 8F 8E D7 
    C4 1A 00 02 1A 76 06 00 2A 02 1F 76 A0 02 3A 07 A9 8A C4 06 06 00 22 76 
    05 8F 2E D2 C4 1A 02 00 1A 76 06 00 04 FE 44 1E 42 A8 25 76 69 FF 84 FE 
    06 00 20 FF 00 72 40 76 24 9E 00 52 FB 60 06 00 22 76 55 9A A9 F4 25 70 
    1A 76 06 00 02 FE 42 1E A9 28 00 08 82 FE 06 00 FF 76 6C CE 67 3E 06 00 
    00 00 
    

    Best,

    Matt

  • Hello,

    I'll further note that if you're still having issues with the attached flash kernel, then there most likely is an issue with the application. Please follow the steps in Section 4.2.2 of this user's guide to ensure everything is set up correctly: https://www.ti.com/lit/ug/sprujh3/sprujh3.pdf

    Best,

    Matt

  • I set up the DCSM as shown in the picture below.
    The cause of the problem is that the BOTDEF3 Flash boot address is set to 0x00088000, which may cause a pause.
    Is there a way to change the starting address in kernel?

  • Hello,

    This shouldn't affect the kernel as it executes from the RAM (and is branched to directly from the Boot ROM). Your application codestart will need to account for 0x88000 flash entry point. I'll also note that LFU flash boot is different from regular flash boot, please note that additional LFU metadata will be required for the bank selection logic (as described in the TRM).

    A few things to check:

    1. I see that you're using GPIO16 and GPIO17 for SCI TX/RX. Please verify that you're calling sciGetFunction(SCI_BOOT_ALT1) in the flash kernel
    2. Please verify that your application's flash sections are 128-bit aligned with ALIGN(8) in the linker cmd file

    Best,

    Matt

  • Boot completed normally after changing to SCI_BOOT_ALT1

    Attached is the Flash.CMD file you requested. Please share the information on LFU metadata required for APP to operate normally

  • Hello,

    Boot completed normally after changing to SCI_BOOT_ALT1

    I'm happy to hear the GPIO change in the kernel resolved the issue!

    Please share the information on LFU metadata required for APP to operate normally

    Please refer to Section 4.8.5 Firmware Update (FWU) Flash Boot in the TRM. If you don't plan to leverage the FWU boot features, please re-configure  the device to use regular flash boot.

    Best,

    Matt