Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: C2000WARE
Hi,
I am using the dual core led example and I see that LED with just one core was blinking faster <1s but when I load both the .out files (I run cpu-1 followed by connect cpu-2 and then load cpu2.out followed by run on cpu-2) the LEDs (both from cpu-1 and cpu-2) blink at much slower rate ~5seconds.
Can you please help me identify what is causing this issue?
On another note, I want to use CPU-1 for motor control and CPU-2 for CAN communication where they both can store/access data/variable. Can you help me point in the right resource/material/training-videos to setup CAN for CPU-2 and also how to store/access data between the two CPUs.
Thanks
Sumeet