This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F29H85X: needs to convert CAN FD example into classic CAN

Part Number: LAUNCHXL-F29H85X
Other Parts Discussed in Thread: SYSCONFIG

I am currently working with the mcan_ex6_transmit_syscfg example and have made the following changes to configure it for Classic CAN, so that the transmitted messages can be viewed in PCAN-View:

  • CAN FD Mode: Disabled
  • Bit Rate Switching: Disabled
  • Nominal Bit Timing Configuration:
    • Prescaler: 9
    • Time Segment 1 (TSEG1): 1
    • Time Segment 2 (TSEG2): 2
    • Synchronization Jump Width (SJW): 2

Despite these changes, I am unable to see any messages in PCAN-View. Could you please confirm whether these settings are correct for Classic CAN operation at 1 Mbps, or advise if any additional configuration is required?