Part Number: TMS320F28P550SJ
Other Parts Discussed in Thread: SYSCONFIG
I have been able to simulate my CLB1 logic and everything works fine. When I go to test it with the hardware, I don't get any ouput from the CLB1. I went ahead and made a test using CLB2.
1 Set CLB2 Input 0 to EPWM1A which is on the LaunchPadXL header.
2. Attached Tile2.
2. Set Tile2 LUT 0 input 0 to Input Boundary 0 with output logic equation i0.
3. Set Tile2 Output Lookup Table 4 input 0 to LUT 0 Output with output logic equation i0.
4. Set CLB Output XBAR to CLB2 Out4 (Mux 12) and assigned GPIO40 which is on the LaunchPadXL header.
When I go ahead and run the program, GPIO40 is constant.
What am I missing?
Thanks
Dennis