This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-POSMGR: Compatibility of BOOSTXL-POSMGR with TMS320F28388D (C2000Ware 5.1.0, TI v22.6.0.LTS Compiler, and ECN1313 EnDat 2.1 Encoder)

Part Number: BOOSTXL-POSMGR
Other Parts Discussed in Thread: TMS320F28388D, C2000WARE

Hello,

I would like to confirm whether the BOOSTXL-POSMGR (Position Manager BoosterPack) can be used with the TMS320F28388D device.

Specifically, I’d like to ask:

  1. Is BOOSTXL-POSMGR supported in C2000Ware v5.1.0?

  2. Is it compatible with projects built using the TI v22.6.0.LTS compiler?

  3. My encoder model is Heidenhain ECN1313, which uses the EnDat 2.1 protocol. Is this encoder supported when using BOOSTXL-POSMGR with F28388D?

  4. If supported, are there any required configuration steps (hardware connections, jumper settings, or firmware modifications) for this setup?

  5. Are there any available example projects or reference codes demonstrating this configuration?

Thank you very much for your assistance.

Best regards,
Jinha