Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: SPI DMA Problems with BURSTSIZE

Part Number: TMS320F28379D
Other Parts Discussed in Thread: SYSCONFIG

I am using the following snippet of code to configure a DMA channel - on an F28379D - to write a buffer of data out to a SPI-addressable DAC device. My intent is to have a single 16-bit element from dac_buffer_a to be written to the peripheral each time the SOCA event triggers.

#define DAC_SPI_TX_DMA_TRIGGER DMA_TRIGGER_EPWM1SOCA
#define DAC_SPI_TX_DMA_ADDRESS ((uint16_t *)(SPIA_BASE + SPI_O_TXBUF))

void DAC_SPI_TX_DMA_init() { 
    DMA_setEmulationMode(DMA_EMULATION_FREE_RUN);
    DMA_configAddresses(DAC_SPI_TX_DMA_BASE, DAC_SPI_TX_DMA_ADDRESS, dac_buffer_a);
    DMA_configBurst(DAC_SPI_TX_DMA_BASE, 1U, 1, 0);
    DMA_configTransfer(DAC_SPI_TX_DMA_BASE, 16U, 0, 0);
    DMA_configMode(DAC_SPI_TX_DMA_BASE, DAC_SPI_TX_DMA_TRIGGER, DMA_CFG_ONESHOT_DISABLE | DMA_CFG_CONTINUOUS_ENABLE | DMA_CFG_SIZE_16BIT);
    DMA_setInterruptMode(DAC_SPI_TX_DMA_BASE, DMA_INT_AT_END);
    DMA_enableInterrupt(DAC_SPI_TX_DMA_BASE);
    DMA_disableOverrunInterrupt(DAC_SPI_TX_DMA_BASE);
    DMA_enableTrigger(DAC_SPI_TX_DMA_BASE);
}

Unfortunately, this is not occurring. At the end of a transfer (16 bytes), inspection of the source address indicates that it did not advance. Why is this the case? My understanding is that passing 1 as the burst size to DMA_configBurst() should result in the source address advancing after each single-word burst. This does not appear to be happening.  

If I change the second argument of DMA_configBurst() from 1 to 2, by the way, the source address ends up as expected (starting address + 16) at the end of the transfer. However, I do not want to send 2 16-bit words each time the triggering event occurs. Rather, I want a single word to be sent.  

  • Hi Brandon,

    Your burst and transfer step sizes all look to be correct. Please send a screenshot of the data type/definition of dac_buffer_a so I can take a look. Also, did you use Sysconfig for this? If so, can you send a screenshot of your Sysconfig selections. And can you add the below line of code to your configurations to make sure wrapping is disabled?

    DMA_configWrap(DAC_SPI_TX_DMA_BASE, 65535U, 0, 65535U, 0);

    Best Regards,

    Delaney