Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000WARE: Does the cpu1 linker look at a previously built cpu2 map?

Part Number: C2000WARE

The following seems to always work: the .map files show that the pointers are correctly shared between the two cpu's but I'm completely baffled how you do it? How does the cpu1 linker know to put those extern pointers into .sharedPtrs section. 

Does the linker for cpu1 look at symbols defined in cpu2 and try to match them up?  I do not have anything in my build command to point the cpu's to each other.

Voodoo !!

cpu1 main.c
extern Uint16 *CBdataProcess;
extern int16 *MB1dataProcess;
extern int16 *MB2dataProcess;

cpu1 link.cmd
.sharedPtrs : > RAMGS12, PAGE = 1

cpu2 main.c
#pragma DATA_SECTION(CBdataProcess,  ".sharedPtrs");
#pragma DATA_SECTION(MB1dataProcess, ".sharedPtrs");
#pragma DATA_SECTION(MB2dataProcess, ".sharedPtrs");
Uint16 *CBdataProcess = 0;
int16 *MB1dataProcess = 0;
int16 *MB2dataProcess = 0;

cpu2 link.cmd
.sharedPtrs : > RAMGS12, PAGE = 1