This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: The status of GPIO when VDDIO / VDD is not powered.

Part Number: TMS320F280039C

Hi Sir,

When the customer was verifying the PMBUS application, they found that when multiple F280039C PMBUS devices are connected, some SLAVE devices are not powered at VDD. However, when SDA, SCL, and GND are still connected to the BUS lines, the SDA and SCL lines are pulled low (from 3.3V to 1.05V). They also verified that other GPIOs exhibit a similar voltage pull-down phenomenon when VDD is not powered. Is there a way to correct this? It is difficult to avoid having unpowered devices on the PMBUS (I2C) bus line.

thanks.