Part Number: TMS320F28386S
Good morning!
I am developing 2 projects with F28386S chip. Prevoiusely I buuilt prototypes and these boards was running fine.
Now I received new pre-production boards, where the XTAL was replaced by 16MHz one by request of customer.
These boards are programmed and run fine with JTAG, but failing to start up on power up or even after asserting XRST. Examining target in CCS I see target is executing in ROM instead of FLASH.
The BOOT0 and BOOT1 pins are driven high.