Part Number: TMS320F28P559SJ-Q1
Hi team,
I ask this for my customer.
1.Because of the limitation of flash size, they would set all the flash sector is unsecure, but set one RAMLS as security.
Then they would copy the code from unsecure flash to secure ram, and use this code to write and read secure variable(some secure variable also in the secure ram, some secure variable in the unsecure flash/ram)
what should be attention in this process(for example, the memcpy function should be placed where? or is it need to unlock the ram during the process)
2.If they use the DCSM_forceFlashErrorStatus to set the SECERRFRC.ERR, what would happen?(generate the interrupt or something else)
BRs
Shuqing