Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: SYSCONFIG, TMDSCNCD28P65X
Hi,
I'm facing an issue while testing the ADCB module on TMS320f28p65. Here's my setup:
- ADC Configuration: Set to 16-bit resolution using SysConfig
- Trigger Source: EPWM18
- Data Transfer: Using DMA
- Input Signal: Constant DC voltage with no observable noise
- REF Voltage: 2.5V external voltage
Despite the input voltage of ADC pin and REF voltage being stable, I'm seeing a fluctuation of about 300 counts in the ADC result. Would you please help me for this problem.