This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000WARE: Ports directory not present in C2000ware 5_05_00

Part Number: C2000WARE

Hi,
The ports directory in lwip is absent C2000ware 5_05_00 onwards. Was this intended? What is the suggested workflow/workaround? This directory contains arch/cc.h which is called in arch.h, and the absence of this directory causes compilation failures.
Thanks in advance
Ganesh

505.png

504.png

  • Hi Ganesh

    The ports folder has been moved out of the lwip stack and it has been moved from

    C:\ti\c2000\C2000Ware_5_04_00_00\libraries\communications\Ethernet\third_party\lwip\lwip-2.1.2\ports  to  C:\ti\c2000\C2000Ware_5_05_00_00\libraries\communications\Ethernet\third_party\lwip\ports

    Best Regards

    Siddharth