Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: Flash API related issue

Part Number: TMS320F28335

Hello TI Team,

I am using a TMS320F28335 controller for my project. I am able to update the firmware successfully using the TI Flash API, and that code runs correctly after reset.

However, when I program the device through Code Composer Studio (CCS) using JTAG, the code runs immediately after loading, but does not run after a power cycle or reset.

It seems like the code is being loaded and executed from RAM instead of Flash. I would like my application to always run from Flash, whether it’s programmed via JTAG or updated via Flash API.

Thanks

  • Hello,

    Can you send the linker cmd file associated with your project? Are you using a flash build configuration?

    Kind regards,

    Skyler

  • /*
    //###########################################################################
    //
    // FILE: F28335.cmd
    //
    // TITLE: Linker Command File For F28335 Device
    //
    //###########################################################################
    // $TI Release: F28335 API Release V2.10 $
    // $Release Date: August 18, 2008 $
    //###########################################################################
    */

    /* ======================================================
    // For Code Composer Studio V2.2 and later
    // ---------------------------------------
    // In addition to this memory linker command file,
    // add the header linker command file directly to the project.
    // The header linker command file is required to link the
    // peripheral structures to the proper locations within
    // the memory map.
    //
    // The header linker files are found in <base>\DSP2833x_Headers\cmd
    //
    // For BIOS applications add: DSP2833x_Headers_BIOS.cmd
    // For nonBIOS applications add: DSP2833x_Headers_nonBIOS.cmd
    ========================================================= */

    /* ======================================================
    // For Code Composer Studio prior to V2.2
    // --------------------------------------
    // 1) Use one of the following -l statements to include the
    // header linker command file in the project. The header linker
    // file is required to link the peripheral structures to the proper
    // locations within the memory map */

    /* Uncomment this line to include file only for non-BIOS applications */
    /* -l DSP2833x_Headers_nonBIOS.cmd */

    /* Uncomment this line to include file only for BIOS applications */
    /* -l DSP2833x_Headers_BIOS.cmd */

    /* 2) In your project add the path to <base>\DSP2833x_headers\cmd to the
    library search path under project->build options, linker tab,
    library search path (-i).
    /*========================================================= */

    /* Define the memory block start/length for the F28335
    PAGE 0 will be used to organize program sections
    PAGE 1 will be used to organize data sections

    Notes:
    Memory blocks on F28335 are uniform (ie same
    physical memory) in both PAGE 0 and PAGE 1.
    That is the same memory region should not be
    defined for both PAGE 0 and PAGE 1.
    Doing so will result in corruption of program
    and/or data.

    L0/L1/L2 and L3 memory blocks are mirrored - that is
    they can be accessed in high memory or low memory.
    For simplicity only one instance is used in this
    linker file.

    Contiguous SARAM memory blocks can be combined
    if required to create a larger memory block.
    */


    MEMORY
    {
    PAGE 0: /* Program Memory */
    /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */

    ZONE0 : origin = 0x004000, length = 0x001000 /* XINTF zone 0 */
    RAML0 : origin = 0x008000, length = 0x001000 /* on-chip RAM block L0 */
    RAML1 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L1 */
    RAML2 : origin = 0x00A000, length = 0x001000 /* on-chip RAM block L2 */
    RAML3 : origin = 0x00B000, length = 0x001000 /* on-chip RAM block L3 */
    ZONE6 : origin = 0x0100000,length = 0x100000 /* XINTF zone 6 */
    ZONE7A : origin = 0x0200000,length = 0x00FC00 /* XINTF zone 7 - program space */
    FLASHH : origin = 0x300000, length = 0x008000 /* on-chip FLASH */
    FLASHG : origin = 0x308000, length = 0x008000 /* on-chip FLASH */
    FLASHF : origin = 0x310000, length = 0x008000 /* on-chip FLASH */
    FLASHE : origin = 0x318000, length = 0x008000 /* on-chip FLASH */
    FLASHD : origin = 0x320002, length = 0x007FFE /* on-chip FLASH */
    FLASHC : origin = 0x328000, length = 0x008000 /* on-chip FLASH */
    FLASHB : origin = 0x330000, length = 0x008000 /* on-chip FLASH */
    FLASHA : origin = 0x338000, length = 0x007F80 /* on-chip FLASH */
    CSM_RSVD : origin = 0x33FF80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
    BEGIN : origin = 0x320000, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
    CSM_PWL : origin = 0x33FFF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */
    OTP : origin = 0x380400, length = 0x000400 /* on-chip OTP */
    ADC_CAL : origin = 0x380080, length = 0x000009 /* ADC_cal function in Reserved memory */

    IQTABLES : origin = 0x3FE000, length = 0x000b50 /* IQ Math Tables in Boot ROM */
    IQTABLES2 : origin = 0x3FEB50, length = 0x00008c /* IQ Math Tables in Boot ROM */
    FPUTABLES : origin = 0x3FEBDC, length = 0x0006A0 /* FPU Tables in Boot ROM */
    ROM : origin = 0x3FF27C, length = 0x000D44 /* Boot ROM */
    RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
    VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */

    PAGE 1 : /* Data Memory */
    /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
    /* Registers remain on PAGE1 */

    BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
    RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */
    RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
    RAML4L5L7 : origin = 0x00C000, length = 0x004000 /* on-chip RAM block L1 */
    // RAML4_L5_ : origin = 0x00C000, length = 0x002000 /* on-chip RAM block L1 */
    // RAML5 : origin = 0x00D000, length = 0x001000 /* on-chip RAM block L1 */
    // RAML6 : origin = 0x00E000, length = 0x001000 /* on-chip RAM block L1 */
    // RAML7 : origin = 0x00F000, length = 0x001000 /* on-chip RAM block L1 */
    ZONE7B : origin = 0x20FC00, length = 0x000400 /* XINTF zone 7 - data space */
    // FLASHB : origin = 0x330000, length = 0x008000 /* on-chip FLASH */
    }

    /* Allocate sections to memory blocks.
    Note:
    codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
    execution when booting to flash
    ramfuncs user defined section to store functions that will be copied from Flash into RAM
    */

    SECTIONS
    {

    /* Allocate program areas: */
    /* The Flash API functions can be grouped together as shown below.
    The defined symbols _Flash28_API_LoadStart, _Flash28_API_LoadEnd
    and _Flash28_API_RunStart are used to copy the API functions out
    of flash memory and into SARAM */

    Flash28_API:
    {
    -lFlash28335_API_V210.lib(.econst)
    -lFlash28335_API_V210.lib(.text)
    } LOAD = FLASHD,
    RUN = RAML0,
    LOAD_START(_Flash28_API_LoadStart),
    LOAD_END(_Flash28_API_LoadEnd),
    RUN_START(_Flash28_API_RunStart),
    PAGE = 0
    .cinit : > FLASHD PAGE = 0
    .pinit : > FLASHD, PAGE = 0
    .text : > FLASHD PAGE = 0
    codestart : > BEGIN PAGE = 0
    ramfuncs : LOAD = FLASHD,
    RUN = RAML0,
    LOAD_START(_RamfuncsLoadStart),
    LOAD_END(_RamfuncsLoadEnd),
    RUN_START(_RamfuncsRunStart),
    PAGE = 0

    csmpasswds : > CSM_PWL PAGE = 0
    csm_rsvd : > CSM_RSVD PAGE = 0

    /* Allocate uninitalized data sections: */
    .stack : > RAMM1 PAGE = 1
    .ebss : > RAML4L5L7 PAGE = 1
    .esysmem : > RAMM1 PAGE = 1

    /* Initalized sections go in Flash */
    /* For SDFlash to program these, they must be allocated to page 0 */
    .econst : > FLASHD PAGE = 0
    .switch : > FLASHD PAGE = 0

    /* Allocate IQ math areas: */
    IQmath : >FLASHD PAGE = 0 /* Math Code */
    IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD
    IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
    FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD

    /* Allocate DMA-accessible RAM sections: */
    DMARAML4 : > RAML4L5L7, PAGE = 1
    DMARAML5 : > RAML4L5L7, PAGE = 1
    DMARAML6 : > RAML4L5L7, PAGE = 1
    DMARAML7 : > RAML4L5L7, PAGE = 1

    /* Allocate 0x400 of XINTF Zone 7 to storing data */
    ZONE7DATA : > ZONE7B, PAGE = 1

    /* .reset is a standard section used by the compiler. It contains the */
    /* the address of the start of _c_int00 for C Code. /*
    /* When using the boot ROM this section and the CPU vector */
    /* table is not needed. Thus the default type is set here to */
    /* DSECT */
    .reset : > RESET, PAGE = 0, TYPE = DSECT
    vectors : > VECTORS PAGE = 0, TYPE = DSECT

    /* Allocate ADC_cal function (pre-programmed by factory into TI reserved memory) */
    .adc_cal : load = ADC_CAL, PAGE = 0, TYPE = NOLOAD

    }

    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */

  • I'm also using DSP2833x_Headers_nonBIOS.cmd file with that Example_flash_Api.cmd file

  • Hi Akash,

    Can you confirm that flash is being programmed by looking at the memory browser after programming?

    Kind regards,

    Skyler

  • yes, flash is programmed hex code is there from starting address,

    one more issue I'm facing that when i write hex file by a flash Api and after writing full hex file when i switch to that firmware code it is not working why.

    what exactly I'm missing in that Hex file. that hex file also not contain an entry point code and also CSM and reserve code

  • Akash,

    Skyler is busy with another project, so I'm going to try and help with your issue.

    I am using a TMS320F28335 controller for my project. I am able to update the firmware successfully using the TI Flash API, and that code runs correctly after reset.

    How are you programming the Flash using the Flash API? Are you using one of our provided Flash kernel/bootloader examples?

    However, when I program the device through Code Composer Studio (CCS) using JTAG, the code runs immediately after loading, but does not run after a power cycle or reset. It seems like the code is being loaded and executed from RAM instead of Flash. I would like my application to always run from Flash, whether it’s programmed via JTAG or updated via Flash API.

    When the code is running, you can halt and check whether code execution is happening from RAM or Flash. You can also export Flash contents after programming "with the Flash API" approach and compare it against Flash contents after programming "using CCS over JTAG" and see if they match. Also, I am assuming that in all cases your device is in Flash boot mode so it boots to Flash after a reset.

    Thanks,

    Sira