This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: Application issues.

Expert 2350 points

Part Number: TMS320F280039C

Hi Team,

According to the specifications, PIN73 should be connected to GND, and at this time, the internal VDD should output 1.2V
But now it's only 0.2V, where is the problem?