Part Number: TMS320F28379D
Dear Sir,
I am using DCL functions 
I have mapped them in RAMLS5. Is it okay to put them RAMLS5 ,and code build without errors?
In flash linker command file where should I put it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28379D
Dear Sir,
I am using DCL functions 
I have mapped them in RAMLS5. Is it okay to put them RAMLS5 ,and code build without errors?
In flash linker command file where should I put it?
hi ,
Yes you can use any of the LSRAMs as long as its available on that device/ variant .
If your using the flash config version and want to use the flash linker cmd file , you can retain these in RAM itself or put it in flash .
Examples used on other devices : flash ://dev.ti.com/tirex/explore/node?node=A__AAto9OmFzGVTSVFxZYK-7g__C2000WARE__1kRFgrO__LATEST
Regards.