This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P550SJ: Compile error when adding a DCL Controller

Part Number: TMS320F28P550SJ
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE

When I add a DCL PI controller to a project that has CLA enabled, I get quite a few error#20s. An example is from DCLF32.h - identifier "DCL_CSS" is undefined.

The project already uses the logger without a problem. I also have added the DCL header and source files paths to the DCL headers and source but still have the problem.

Please advise how to solve the problem.

Thanks

Dennis