Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: TMDXIDDK379D, C2000WARE
Hello TI Team,
I am working with the F28379D LaunchPad and the 3-phase GaN inverter board for a dual-motor control application. I am using MotorControlSDK 5_03 as the base reference.
I have integrated a BiSS-C absolute encoder into the dual-axis motor control code. The BiSS-C interface itself is working correctly, and the angle reading is verified in open-loop and FCL Level-2. However, when I integrate the BiSS-C angle into the FCL closed-loop control (Level-3 to Level-5), the system does not behave correctly.
Issue description:
- The motor starts normally in closed loop.
- After a short time, the speed gradually reduces without any command change.
- Eventually the speed reaches near zero (approximately 0.0001 pu), but the motor never stops completely.
- Current continues to flow even though the speed reference is unchanged.
- This behavior is consistent across FCL Level-3, Level-4, and Level-5.
Debug steps already tried:
- The same hardware works correctly with incremental encoder example and FCL Level-3/4.
- BiSS-C angle is verified in FCL Level-2, and the motor runs normally there.
- Added manual angle delay compensation — issue still persists.
- Tested with speed observer and angle estimator for compensation — no improvement.
- Verified position data and CRC from BiSS-C — all correct.
Thank you for your support.
Regards,
divyesh patel