This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: Can we use MCAN as a boot?

Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE

Hello TI Team,

I am seeking clarification regarding the TMS320F28388's bootloader capabilities, as the Technical Reference Manual lists "CAN A" as a boot source. Given that this device features the MCAN-A peripheral instead of the older eCAN, I need to confirm if this "CAN A" boot mode actually utilizes the MCAN-A peripheral. If it does, I also need to know whether the boot-ROM supports firmware loading via CAN-FD frames or if it is restricted to classic CAN 2.0B frames, and what the default GPIO pins are for this boot mode.