Part Number: TMS320F280039
Other Parts Discussed in Thread: SYSCONFIG
Hello,
We are using F280039 100 pin (PZ) package in one of our designs.
I need clarification on the following:
How are the 2 ADC pins B5 (pin 32), B11 (pin 30) internally coupled with the GPIO pins B5GPIO20 (pin 48) and B11GPIO21 (pin 49)? Can I use pins 32 and 30 for analog inputs (ADC inputs B5 and B11) and simultaneously use pins 48 and 49 as GPIO? If that is possible, how to configure them in the code?
When I tried to configure the 4 pins as intended using .syscfg file, I get a "resource conflict" error message.
With regards,
Vijay Limaye