Part Number: TMS320F2800157
Other Parts Discussed in Thread: DRV8353, C2000WARE, MOTORWARE, TMS320F28069F, TMS320F28069M
Hello Team,
We are working on a customised board with the F2800157. Initially, development was done using the F2800157 LaunchPad + DRV8353.
I need to rotate the flywheel magneto for just 2 or 3 revolutions when the user requests it. Do I need to use FOC for this, or is there any shortcut method to rotate the flywheel magneto for only 2–3 revolutions? Currently, I am facing an issue where the flywheel is not able to run under load.
For running under load, which parameters are more important — inertia, starting current, or open-load start? On which aspect should I focus more?
Please support on this topic. Currently, it is not running properly and is swinging back and forth with only half rotation. I have attached the video.
Thank you
Regards
C.Prabhakaran