Part Number: LAUNCHXL-F28P65X
Other Parts Discussed in Thread: DAC128S085EVM,
Hi,
I connected the DAC128S085EVM to the LAUNCHXL-F28P65X Board. I installed the required Jumpers, bended J5-42 and connected JA-2 to JB-2 using a jumper wire.
When DAC128S_ENABLE is not enabled and the DAC128S085EVM installed, no error occurs when running the Motor.
The Problem occurs, when i enable DAC128S_ENABLE and start the Motor. The first few seconds, the currentUnbalance bit turns to 1. After a few seconds, ModuleOverCurrent sets to 1. The Motor never starts to actually spin with the Predefine DAC128S_ENABLE.