This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P650DH: Could DCSM locks DRAM (TRM desciprtion not aligned)

Part Number: TMS320F28P650DH

Hi Experts,

Could DCSM locks DRAM? The description in TRM is confusion.

1 The description only includes LSsRAM

image.png

But I can see the DRAM selection in GTABRAM1 register.

 

In the meantime, it's also cunfsusing that if the DCSM has GRABSECT2

The GRABRAM2 register is shown as "reserved"

image.png

3 In the register map, there is a description for GRARAM2image.png