This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F29H850TU: CCS 20.4 - insert hardware breakpoint in RAM?

Part Number: F29H850TU

I have a breakpoint set in code that is copied from flash to RAM.  CCS uses a SW breakpoint since the code is in RAM - but the SW breakpoint opcode is overwritten whenever the device is reset.

I've been toggling the breakpoint off/on before I run from main (i.e. reset --> restart --> manually toggle breakpoint off and back on --> run) The copy from flash is done before this point. 

Is there a way to force the use of a HW breakpoint in this case? Or a way to automatically toggle any set breakpoint off and back on after a restart?