Part Number: TMS320F28379D
Hello,
I am developing a custom Bootloader for the TMS320F28379D and I am facing an issue with preserving a status flag in RAM across a software reset.
I need to pass a "Boot Flag" from the Main Application to the Bootloader to force an update mode.
-
Application writes a magic value to a shared variable in RAM.
-
Application triggers a software reset using
SysCtl_resetDevice(). -
Bootloader starts, checks the variable, and stays in boot mode if the magic value is present.
Even though I have defined the section as type = NOINIT in the Linker Command File, the variable appears to be re-initialized (cleared to 0) or overwritten after the software reset. When the Bootloader reads it, the value is gone.
My Implementation:
1. C Code (Declaration): I am using #pragma NOINIT and ensuring the variable is not explicitly initialized in the code.

2. Linker Command File (.cmd): I mapped the section to RAM_EXCHANGE in Global Shared RAM on PAGE 1.


My Questions:
-
Is there any mechanism in the standard TI
_c_int00startup routine that might override theNOINITattribute for sections in GS RAM? -
Does the device Boot ROM execution (which runs immediately after the reset and before my Bootloader) use or clear specific areas of the RAMGSx, potentially overwriting my flag?
-
Is there a recommended "safe" RAM location for persistent flags across software resets on the F2837xD?
Any advice on how to keep this data persistent would be appreciated.
Thank you.