Part Number: TMS320F28P650DK
Dear Expert,
As below struct, if CPU1 and CLA do bitwise write operation on this struct(such as CPU1 write to test_1 and CLA write to test_2) at the same time. This will manipulate test_3 value. How to avoid this scenario? Could you provide a guidance on how to handle the struct that shared with CPU1 and CLA?
typedef union
{
uint32_t flags;
struct
{
uint32_t test_1 : 1;
uint32_t test_2 : 1;
uint32_t test_3 : 1;
uint32_t reserved : 30;
}bit;
}TESTFLAGS;
Best Regards!
Jacob