Part Number: TMS320F28P559SJ-Q1
Hi,
The content of the Analog Subsystem block diagram image (Figure 14-1. Analog Subsystem Block Diagram) and the related tables (Table 14-1 & 14-4) in the TMS320F28P55x Technical Reference Manual (TRM) seem to be inconsistent. (Based on the 128-pin PDT package)
For instance, Figure 14-1 indicates that the A12 channel is selected for HPMXSEL0 of the CMPSS-2 Input Mux.
However, Tables 14-1 and 14-4 indicate that this setting selects the A4 / B8 channels for the HP input of the CMPSS-2 module.
Which one is correct?
Furthermore, while Tables 14-1 and 14-4 provide some understanding of how the Analog Subsystem's input ports are connected to the ADC, CMPSS, DAC, and PGA modules, there doesn't seem to be an image or table that specifically details the exact configuration of the external A/D input channels and other internal connections through the built-in 32-channel multiplexer of each ADC module, from ADC-A through ADC-E. Is there any documentation available for this?
Best regards,
Sang-il