This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Runtime issue with universal Lab code for f28379d

Part Number: TMS320F28379D

Hi,

I have ported the universal lab code to f28379d. 

While running, the CPU gets stuck at Flash_initModule() function. 

Looks like an issue with the memory map. I have defined __TI_EABI__

Please let me know what I can do to address this issue.

 

//#############################################################################
//
// FILE:    dual_axis_f2837x_flash_lnk_cpu1.cmd.cmd
//
//#############################################################################

CLA_SCRATCHPAD_SIZE = 0x100;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start
#endif //CLA_C


MEMORY
{
    /* BEGIN is used for the "boot to Flash" bootloader mode   */
   BEGIN            : origin = 0x080000,   length = 0x000002
   BOOT_RSVD        : origin = 0x000002,   length = 0x000121     /* Part of M0, BOOT rom will use this for stack */
   RAMM0           	: origin = 0x000123,   length = 0x0002DD
   RAMM1            : origin = 0x000400,   length = 0x0003F8     /* on-chip RAM block M1 */
/* RAMM1_RSVD       : origin = 0x0007F8,   length = 0x000008 */  /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

   RAMD0           	: origin = 0x00B000,   length = 0x000800
   RAMD1            : origin = 0x00B800,   length = 0x000800

   RAMLS0          	: origin = 0x008000,   length = 0x000800
   RAMLS1          	: origin = 0x008800,   length = 0x000800
   RAMLS2      		: origin = 0x009000,   length = 0x000800
   RAMLS3      		: origin = 0x009800,   length = 0x000800
   RAMLS4      	    : origin = 0x00A000,   length = 0x000800
   RAMLS5           : origin = 0x00A800,   length = 0x000800

   // RAMGS0           : origin = 0x00C000,   length = 0x001000
   // RAMGS1           : origin = 0x00D000,   length = 0x001000
   RAMGS0_1           : origin = 0x00C000,   length = 0x002000
   RAMGS2           : origin = 0x00E000,   length = 0x001000
   RAMGS3           : origin = 0x00F000,   length = 0x001000
   RAMGS4           : origin = 0x010000,   length = 0x001000
   RAMGS5           : origin = 0x011000,   length = 0x001000
   RAMGS6           : origin = 0x012000,   length = 0x001000
   RAMGS7           : origin = 0x013000,   length = 0x001000
   RAMGS8           : origin = 0x014000,   length = 0x001000
   RAMGS9           : origin = 0x015000,   length = 0x001000
   RAMGS10          : origin = 0x016000,   length = 0x001000

/* RAMGS11          : origin = 0x017000, length = 0x000FF8 */  /* Uncomment for F28374D, F28376D devices */
/* RAMGS11_RSVD     : origin = 0x017FF8, length = 0x000008 */  /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

   RAMGS11          : origin = 0x017000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
   RAMGS12          : origin = 0x018000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
   RAMGS13          : origin = 0x019000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
   // RAMGS14          : origin = 0x01A000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
   // RAMGS15          : origin = 0x01B000, length = 0x000FF8     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
   RAMGS1415          : origin = 0x01A000, length = 0x001FF8     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
/* RAMGS15_RSVD     : origin = 0x01BFF8, length = 0x000008 */  /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
                                                               /* Only on F28379D, F28377D, F28375D devices. Remove line on other devices. */

   /* Flash sectors */
   FLASHA           : origin = 0x080002,   length = 0x001FFE	/* on-chip Flash */
   FLASHB           : origin = 0x082000,   length = 0x002000	/* on-chip Flash */
   FLASHC           : origin = 0x084000,   length = 0x002000	/* on-chip Flash */
   FLASHD           : origin = 0x086000,   length = 0x002000	/* on-chip Flash */
   FLASHE           : origin = 0x088000,   length = 0x008000	/* on-chip Flash */
   FLASHF           : origin = 0x090000,   length = 0x008000	/* on-chip Flash */
   FLASHG           : origin = 0x098000,   length = 0x008000	/* on-chip Flash */
   FLASHH           : origin = 0x0A0000,   length = 0x008000	/* on-chip Flash */
   FLASHI           : origin = 0x0A8000,   length = 0x008000	/* on-chip Flash */
   FLASHJ           : origin = 0x0B0000,   length = 0x008000	/* on-chip Flash */
   FLASHK           : origin = 0x0B8000,   length = 0x002000	/* on-chip Flash */
   FLASHL           : origin = 0x0BA000,   length = 0x002000	/* on-chip Flash */
   FLASHM           : origin = 0x0BC000,   length = 0x002000	/* on-chip Flash */
   FLASHN           : origin = 0x0BE000,   length = 0x001FF0	/* on-chip Flash */
/* FLASHN_RSVD      : origin = 0x0BFFF0,   length = 0x000010 */ /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */


   RESET           	: origin = 0x3FFFC0, length = 0x000002

   CPU2TOCPU1RAM    : origin = 0x03F800, length = 0x000400
   CPU1TOCPU2RAM    : origin = 0x03FC00, length = 0x000400

   CANA_MSG_RAM     : origin = 0x049000,   length = 0x000800
   CANB_MSG_RAM     : origin = 0x04B000,   length = 0x000800

   CLA1_MSGRAMLOW   : origin = 0x001480,   length = 0x000080
   CLA1_MSGRAMHIGH  : origin = 0x001500,   length = 0x000080
}

SECTIONS
{
   codestart           : > BEGIN, ALIGN(4)
   .text               : >> FLASHA | FLASHB | FLASHC | FLASHD, ALIGN(4)
   .cinit              : > FLASHG, ALIGN(4)
   .switch             : > FLASHG, ALIGN(4)
   .reset              : > RESET, TYPE = DSECT /* not used, */
   .stack              : > RAMM1

#if defined(__TI_EABI__)
   .init_array      : > FLASHG, ALIGN(8)
   .bss             : > RAMLS0 | RAMLS1, ALIGN(4)
   .bss:output      : > RAMLS0 | RAMLS1
   .bss:cio         : > RAMLS0 | RAMLS1
   .data            : > RAMLS0 | RAMLS1
   .sysmem          : > RAMLS0 | RAMLS1
   /* Initalized sections go in Flash */
   .const           : > FLASHG, ALIGN(8)
#else
   .pinit           : > FLASHG, ALIGN(8)
   .ebss            : > RAMLS0 | RAMLS1
   .esysmem         : > RAMLS0 | RAMLS1
   .cio             : > RAMLS0 | RAMLS1
   /* Initalized sections go in Flash */
   .econst          : > FLASHG, ALIGN(8)
#endif

   MSGRAM_CPU1_TO_CPU2 : > CPU1TOCPU2RAM, type=NOINIT
   MSGRAM_CPU2_TO_CPU1 : > CPU2TOCPU1RAM, type=NOINIT

    /* CLA specific sections */
#if defined(__TI_EABI__)
   Cla1Prog         :   LOAD = FLASHF,
                        RUN = RAMLS4 | RAMLS5,
                        LOAD_START(Cla1funcsLoadStart),
                        LOAD_END(Cla1funcsLoadEnd),
                        RUN_START(Cla1funcsRunStart),
                        LOAD_SIZE(Cla1funcsLoadSize),
                        ALIGN(8)
#else
   Cla1Prog         :   LOAD = FLASHF,
                        RUN = RAMLS4 | RAMLS5,
                        LOAD_START(_Cla1funcsLoadStart),
                        LOAD_END(_Cla1funcsLoadEnd),
                        RUN_START(_Cla1funcsRunStart),
                        LOAD_SIZE(_Cla1funcsLoadSize),
                        ALIGN(8)
#endif

   ClaData			: > RAMLS3

   Cla1ToCpuMsgRAM  : > CLA1_MSGRAMLOW, type=NOINIT
   CpuToCla1MsgRAM  : > CLA1_MSGRAMHIGH, type=NOINIT

   /* SFRA specific sections */
   SFRA_F32_Data	: > RAMGS5, ALIGN = 64
   sfra_data    	: > RAMGS5

#ifdef CLA_C
   /* CLA C compiler sections */
   //
   // Must be allocated to memory the CLA has write access to
   //
   CLAscratch       :
                     { *.obj(CLAscratch)
                     . += CLA_SCRATCHPAD_SIZE;
                     *.obj(CLAscratch_end) } >  RAMLS2

   .scratchpad      : > RAMLS2
   .bss_cla         : > RAMLS2

#if defined(__TI_EABI__)
   .const_cla       :   LOAD = FLASHF,
                        RUN = RAMLS4,
                        RUN_START(Cla1ConstRunStart),
                        LOAD_START(Cla1ConstLoadStart),
                        LOAD_SIZE(Cla1ConstLoadSize),
                        ALIGN(8)
#else
   .const_cla       :   LOAD = FLASHF,
                        RUN = RAMLS4,
                        RUN_START(Cla1ConstRunStart),
                        LOAD_START(Cla1ConstLoadStart),
                        LOAD_SIZE(Cla1ConstLoadSize),
                        ALIGN(8)
#endif
#endif //CLA_C

#if defined(__TI_EABI__)
   .TI.ramfunc : {} LOAD = FLASHE,
                  //   RUN = RAMGS0 | RAMGS1 | RAMGS2 | RAMGS3,
                  RUN = RAMGS0_1 | RAMGS2 | RAMGS3,
                    LOAD_START(RamfuncsLoadStart),
                    LOAD_SIZE(RamfuncsLoadSize),
                    LOAD_END(RamfuncsLoadEnd),
                    RUN_START(RamfuncsRunStart),
                    RUN_SIZE(RamfuncsRunSize),
                    RUN_END(RamfuncsRunEnd),
                    ALIGN(4)
#else
   .TI.ramfunc : {} LOAD = FLASHE,
                  //   RUN = RAMGS0 | RAMGS1 | RAMGS2 | RAMGS3,
                  RUN = RAMGS0_1 | RAMGS2 | RAMGS3,
                    LOAD_START(_RamfuncsLoadStart),
                    LOAD_SIZE(_RamfuncsLoadSize),
                    LOAD_END(_RamfuncsLoadEnd),
                    RUN_START(_RamfuncsRunStart),
                    RUN_SIZE(_RamfuncsRunSize),
                    RUN_END(_RamfuncsRunEnd),
                    ALIGN(4)
#endif
GROUP
   {
    .TI.ramfunc
     ramfuncs
     dclfuncs
     dcl32funcs
    }
    						         LOAD >  FLASHG,
                              RUN  >  RAMGS1415,
                              LOAD_START(RamfuncsLoadStart),
                              LOAD_END(RamfuncsLoadEnd),
                              LOAD_SIZE(RamfuncsLoadSize),
                              RUN_START(RamfuncsRunStart),
                              RUN_END(RamfuncsRunEnd),
                              RUN_SIZE(RamfuncsRunSize),
                              ALIGN(8)
    ctrlfuncs            :    LOAD >  FLASHG,
                              RUN  >  RAMGS1415,
                              LOAD_START(loadStart_ctrlfuncs),
                              LOAD_END(loadEnd_ctrlfuncs),
                              LOAD_SIZE(loadSize_ctrlfuncs),
                              RUN_START(runStart_ctrlfuncs),
                              RUN_END(runEnd_ctrlfuncs),
                              RUN_SIZE(runSize_ctrlfuncs),
                              ALIGN(8)

   //  .binit                : >  FLASHG,
   //                            ALIGN(8)
   //  .cinit                : >  FLASHA,
   //                            ALIGN(8)
   //  .stack                : >  RAMM0
   //  .init_array           : >  FLASHA,
   //                            ALIGN(8)
   //  .bss                  : >  RAMD0
   //  .const                : >  FLASHA,
   //                            ALIGN(8)
   //  .data                 : >  RAMD0
   //  .switch               : >  FLASHA,
   //                            ALIGN(8)
   //  .sysmem               : >  RAMD0


   est_data             : >  RAMGS13,
                              LOAD_START(loadStart_est_data),
                              LOAD_END(loadEnd_est_data),
                              LOAD_SIZE(loadSize_est_data)

    hal_data             : >  RAMD1,
                              LOAD_START(loadStart_hal_data),
                              LOAD_END(loadEnd_hal_data),
                              LOAD_SIZE(loadSize_hal_data)

    user_data            : >  RAMD1,
                              LOAD_START(loadStart_user_data),
                              LOAD_END(loadEnd_user_data),
                              LOAD_SIZE(loadSize_user_data)

    foc_data             : >  RAMD1,
                              LOAD_START(loadStart_foc_data),
                              LOAD_END(loadEnd_foc_data),
                              LOAD_SIZE(loadSize_foc_data)

    sys_data             : >  RAMD1,
                              LOAD_START(loadStart_sys_data),
                              LOAD_END(loadEnd_sys_data),
                              LOAD_SIZE(loadSize_sys_data)

    vibc_data            : >  RAMGS12,
                              LOAD_START(loadStart_vibc_data),
                              LOAD_END(loadEnd_vibc_data),
                              LOAD_SIZE(loadSize_vibc_data)

    dmaBuf_data          : >  RAMGS12,
                              LOAD_START(loadStart_dmaBuf_data),
                              LOAD_END(loadEnd_dmaBuf_data),
                              LOAD_SIZE(loadSize_dmaBuf_data)

    datalog_data         : >  RAMGS12,
                              LOAD_START(loadStart_datalog_data),
                              LOAD_END(loadEnd_datalog_data),
                              LOAD_SIZE(loadSize_datalog_data)

    SFRA_F32_Data        : >  RAMGS12,
                              LOAD_START(loadStart_SFRA_F32_Data),
                              LOAD_END(loadEnd_SFRA_F32_Data),
                              LOAD_SIZE(loadSize_SFRA_F32_Data)

}

//===========================================================================
// End of file.
//===========================================================================
  • Hello,

    Can you confirm that Flash_initModule is being executed from RAM? Which line is your code hanging on? Does execution remain in this function or go to an interrupt handler?

    Best,

    Alex

  • Hi Alex,

    The functions runs from the RAM.

    This is the output from the map file-
    .TI.ramfunc 
    *          0    00088000    00001169     RUN ADDR = 0000c000
                      00088000    0000072e     fast_full_lib_eabi.lib : est_flib_priv.obj (.TI.ramfunc:EST_runEst)
                      0008872e    0000052c     motor1_drive.obj (.TI.ramfunc:motor1CtrlISR)
                      00088c5a    00000213     fast_full_lib_eabi.lib : est_all_identify_flib_priv.obj (.TI.ramfunc:EST_configureTrajState)
                      00088e6d    000000b4                            : est_flib_priv.obj (.TI.ramfunc:EST_run)
                      00088f21    0000007f                            : est_all_run_flib_priv.obj (.TI.ramfunc:EST_setupTrajState)
                      00088fa0    0000005d                            : est_Traj_flib_priv.obj (.TI.ramfunc:EST_Traj_run)
                      00088ffd    00000043     driverlib_eabi.lib : flash.obj (.TI.ramfunc:Flash_initModule)
                      00089040    0000002c                        : flash.obj (.TI.ramfunc:Flash_setBankPowerMode)
                      0008906c    00000024                        : flash.obj (.TI.ramfunc:Flash_setWaitstates)
                      00089090    0000001d                        : flash.obj (.TI.ramfunc:Flash_setPumpPowerMode)
                      000890ad    00000018                        : flash.obj (.TI.ramfunc:Flash_disableCache)
                      000890c5    00000018                        : flash.obj (.TI.ramfunc:Flash_disablePrefetch)
                      000890dd    00000017                        : flash.obj (.TI.ramfunc:Flash_enableCache)
                      000890f4    00000017                        : flash.obj (.TI.ramfunc:Flash_enablePrefetch)
                      0008910b    00000016     fast_full_lib_eabi.lib : est_flib_priv.obj (.TI.ramfunc:EST_doSpeedCtrl)

    The execution enters the function as seen below

    Upon stepping through into the Flash_initModule(), the CALL STACK shows 0x3FE468 and the control of execution gets stuck.

    I have modified the 'flash.c' file with warning symbols to check which section of _defined is active. The execution reaches Line 17 at '#warn("CPP is defined");' and gets stuck.

    #include "flash.h"
    
    #ifndef __cplusplus
    #warn("CPP is not defined");
    #pragma CODE_SECTION(Flash_initModule, ".TI.ramfunc");
    #pragma CODE_SECTION(Flash_powerDown, ".TI.ramfunc");
    #pragma CODE_SECTION(Flash_wakeFromLPM, ".TI.ramfunc");
    #endif
    
    //*****************************************************************************
    //
    // Flash_initModule
    //
    //*****************************************************************************
    #ifdef __cplusplus
    #pragma CODE_SECTION(".TI.ramfunc");
    #warn("CPP is defined");
    #endif

  • Hello,

    It looks like your device is getting reset on executing this line. Can you please share the contents of the reset cause (RESC) register?
    Best,

    Alex

  • Hi Alex,

    The issue was the mapping.

    I have fixed it.

  • Hello,

    Glad to hear you resolved your issue. I will go ahead and close this thread.

    Best,

    Alex