Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: CLB input and output connection

Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE, SYSCONFIG,

CLB has 8 inputs and 16 outputs, these port can be set in the CLB configuration as the following pic

e462ed6ec64b0c2ad63a8b5930cfae0e.png

but in the attached tile, both the lut, fsm and counter can only use boundary input as input port and output lut as output port. does the boundary inputx link to CLB inputx and the output lut's destination links to overiding outputs? could you explain the correponding mapping relationship? in this mode boundary inputs are not used as simulation inputs and they are connected to the clb input ports.

also the clb output signal may pass to epwm xbar, if i can choose the source with the mux configuration?

cfaf34ec3b2cdc5e51ace12a661d9886.png