Part Number: TMS320F28P550SJ
Hi Champs,
Now my customer found a MCU failure during the prototype stage, detailed as follows:
1. The prototype suddenly shut down during operation, and the temperature-monitoring F28P550 rapidly increased from 86℃ to 114℃;
2. Test the power consumption of the prototype when standby. The total power input is 8W (normally it is 2.2W), and the input power without DSP supply is 1.6W;
3. Test the overheating F28P550, its ADC and EPWM function are both normal;
4. After replacing the F28P550, the prototype's power consumption returned to normal.
The customer want to know why this heating phenomenon occurs, because the ADC and EPWM modules are working normally, the customer suspects that there might be some internal short circuit in the F28P550. Could you help to check this?
Thanks!
Best regards,
Julia