Part Number: CCSTUDIO-THEIA
Other Parts Discussed in Thread: TMDSCNCD28388D
I am currently evaluating the TMDSCNCD28388D using the onboard XDS100V2 and CCS 20.4.0.13.
I am using the standard examples:
-
led_ex1_c28x_cm_blinky_cpu1 -
led_ex1_c28x_cm_blinky_cm
Status: Both projects load and run correctly in standalone mode (both LEDs blink).
The Issue: Debugging CPU1 works perfectly. However, when I debug the CM core, I lose control over the GPIOs. Even though the connection to the CM is established, I cannot toggle the pins. It appears that CPU1 retains or takes back the GPIO master ownership during the CM debug session.