This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS3.3, TMS320F28027, Flash API Error #-1

Other Parts Discussed in Thread: TMS320F28027

 Dear all,

i have a problem with CCS 3.3.82.13: If i try to flash an TMS320F28027, an error occurs: "Flash API Error #-1"

This happens only with TMS devices, TMX devices are working well!

I could fix the problem when using a new Flash API from CCS4 (FlashAPIInterface2802xV2_00.out).

Because i don't want to change the whole toolset in this project, i'm using the API with CCS3.3.

Is this OK, or should i use another API, especially made for CCS3.3?

Thanks for answering my Question

Christoph