This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P550SJ: tmp file errors

Part Number: TMS320F28P550SJ

I am upgrading an existing 28035 project to use a 28p550. The old project used bit-field but I would like to use driverlib on the new project. Since there are numerous bit-field statements, I needed to use both driverlib and bit-field. I have been able to install both including the compiler symbol _DUAL_HEADERS. Things seem to be working but I am getting errors on the CLATask assembly file. They reference tmp files but I can not find them on my machine which is a Mac. Here are some of the errors.

Assembly errors.rtf  

Please help on how to resolve errors that are in tmp files. Also, are the errors caused since I have both bit-field and driverlib active/

Thanks

Dennis