Part Number: TMS320F28035-EP
Dear Team,
I try to perform basic SEE analysis on "TMS320F28035MPNTEP". Could you please share the cross section area of inernal memory regions?
Best Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28035-EP
Dear Team,
I try to perform basic SEE analysis on "TMS320F28035MPNTEP". Could you please share the cross section area of inernal memory regions?
Best Regards.
Hi,
Please see the memory section on page 44 to see the allocation.
https://www.ti.com/lit/gpn/tms320f28035-ep
Regards,
Ozino
Dear Ozino,
Thanks for your reply.
I need the physical cross-sectional area of the internal memory regions, expressed in mm² or cm².
Best Regards.
Hi Ersin,
I have reassigned this thread to someone with expertise in this matter, however due to the holiday season they will be out for the next week or so. We appreciate your patience in this matter.
Kind regards,
AJ Favela
Ersin,
Sorry for the long delay, I've been out for a bit. I'm looking into this with our design team. This is something we should be able to provide, just need to find the right output file on my end.
Best,
Matthew
Ersin,
Wanted to reply back, this is taking a bit longer than I anticipated. I'm still looking into this however, and will give another update by end of the week.
Best,
Matthew
Dear Matthew,
Thank you for your interest.
I look forward to your response.
Best regards,
Dear Matthew,
I hope you are doing well.
I would appreciate it if you could kindly respond at your earliest convenience, as our timeline is becoming critical.
Best Regards.
Ersin,
Thanks for your patience, due to the age of this device its taking longer than I anticipated to extract this info. Hopefully I can get you some numbers by next week.
Best,
Matthew
Ersin,
Please refer to the below:
| Memory Name | Address Range | Area(sq mm) |
| M0 | 0x0000 - 0x03FF | 0.357 |
| M1 | 0x0400 - 0x07FF | 0.357 |
| PIE | 0x0D00 - 0x0DFF | 0.205 |
| CLA Message | 0x1500 - 0x157F | 0.180 |
| CAN | 0x6040-0x60FF | 0.193 |
| CAN | 0x6100-0x61FF | 0.205 |
| L0 | 0x8000 - 0x87FF | 0.559 |
| L1 | 0x8800 - 0x8BFF | 0.357 |
| L2 | 0x8C00 - 0x8FFF | 0.357 |
| L3 | 0x9000 - 0x9FFF | 0.963 |
Best,
Matthew
Dear Matthew,
Thanks for your reply.
Could you please share the cross-sectional areas of the other memory regions, along with their register counts?
Ersin,
Thanks for the follow-up request. Unfortunately, we're unable to support this level of expanded analysis at this time.
If you require further support I would request you to reach out to our sales team to discuss this opportunity further so that we can align on the resource need in this case.
Best,
Matthew