Part Number: TMS320F28P650SH
Other Parts Discussed in Thread: C2000WARE
The thing is We designed a coustom Evaluation Board using TMS320F28P650SH6 176 pin controller IC , The Hardware Design Parameters are right(We have used same design in f280039c control card) , the issue is adc pins are only reading either 0 or 3896, say 2.5 volts present on the pin(Verified using multimeter) the Result register is not reading
it goes 4096 above 2.5 volts,
0 below 2.5 volts,
that to i am using example soc trigger code ,
even timer triggered code is giving same output. Any assistance please i am using sdk 5.04, i am using exact example code ,
I tried with changing Vref 2.5 and 3.3 same thing is happening,
Also tried External Reference voltage (Accordingly changed Vref setting as well)- Same thing is happening.
My schematic of the board