Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: MCU reset

Part Number: TMS320F28379D
Other Parts Discussed in Thread: UNIFLASH

Hello Forms,


When testing with sinePWM using Incremental angle. MCU stopped working, when checked MCU set is happening at 100Hz(10ms), with Off Duration of 55.2us.

Reference Images: 
A) Full Reset Image
Channel1 : VDD3V 
Channel2 : MCU-RST 
b1d0ff0a-8592-417b-8934-7a9b33b3e1b7.jpg

B) Off time Reset Image:
Channel1 : VDD3V 
Channel2 : MCU-RST 
2fa1ad8a-f4c7-416f-962c-19c015a750e2.jpg

B) Wrt to Oscilloscope Image:
Channel1 : VDD3V 
Channel2 : MCU-RST 
Channel3 : External Oscillator
b1dfb5e1-2895-4cf5-98a6-59622f461294.jpg


Thanks in advance,
Soumitri Kumar.

  • Hello Forms,

    In the above scenario,

    I wasn't able to Find the MCU Reset now but unable to flash code into it. When Connected to flash code into it using XDS100v2, it shows following errors.

    Where,
    Channel 1 : MCU Core Voltage  - 1.2V
    Channel 2 : MCU Reset Signal  -  3.3V
    Channel 3 : MCU Input Voltage  - 3.3V

     

    Errors as Follows.


    To solve the above I tried to reduce the JTAG Clock Frequency to 500kHz and tried, it didn't connect either using CCS as well as UniFlash.
    CCS Configuration :



    So I tried using with "Test Connection " whether the Problem is it with Board/ Programmer.

    Below are the Results of it.

    -----[Print the board config pathname(s)]------------------------------------ C:\Users\LENOVO~1\AppData\Local\TEXASI~1\ CCS\ccs2011\0\0\BrdDat\testBoard.dat -----[Print the reset-command software log-file]----------------------------- This utility has selected a 100/110/510 class product. This utility will load the adapter 'jioserdesusb.dll'. The library build date was 'Mar 19 2025'. The library build time was '10:02:15'. The library package version is '20.1.0.3429'. The library component version is '35.35.0.0'. The controller does not use a programmable FPGA. The controller has a version number of '4' (0x00000004). The controller has an insertion length of '0' (0x00000000). This utility will attempt to reset the controller. This utility has successfully reset the controller. -----[Print the reset-command hardware log-file]----------------------------- The scan-path will be reset by toggling the JTAG TRST signal. The controller is the FTDI FT2232 with USB interface. The link from controller to target is direct (without cable). The software is configured for FTDI FT2232 features. The controller cannot monitor the value on the EMU[0] pin. The controller cannot monitor the value on the EMU[1] pin. The controller cannot control the timing on output pins. The controller cannot control the timing on input pins. The scan-path link-delay has been set to exactly '0' (0x0000). -----[The log-file for the JTAG TCLK output generated from the PLL]---------- There is no hardware for programming the JTAG TCLK frequency. -----[Measure the source and frequency of the final JTAG TCLKR input]-------- There is no hardware for measuring the JTAG TCLK frequency. -----[Perform the standard path-length test on the JTAG IR and DR]----------- This path-length test uses blocks of 64 32-bit words. The test for the JTAG IR instruction path-length failed. The many-ones then many-zeros tested length was 1760 bits. The many-zeros then many-ones tested length was -2016 bits. The test for the JTAG DR bypass path-length failed. The many-ones then many-zeros tested length was 1472 bits. The many-zeros then many-ones tested length was -2016 bits. -----[Perform the Integrity scan-test on the JTAG IR]------------------------ This test will use blocks of 64 32-bit words. This test will be applied just once. Do a test using 0xFFFFFFFF. Scan tests: 1, skipped: 0, failed: 0 Do a test using 0x00000000. Test 2 Word 0: scanned out 0x00000000 and scanned in 0xFFFFFFFF. Test 2 Word 1: scanned out 0x00000000 and scanned in 0xFFFFFFFF. Test 2 Word 2: scanned out 0x00000000 and scanned in 0xFFFFFFFF. Test 2 Word 3: scanned out 0x00000000 and scanned in 0xFFFFFFFF. Test 2 Word 4: scanned out 0x00000000 and scanned in 0xFFFFFFFF. Test 2 Word 5: scanned out 0x00000000 and scanned in 0xFFFFFFFF. Test 2 Word 6: scanned out 0x00000000 and scanned in 0xFFFFFFFF. Test 2 Word 7: scanned out 0x00000000 and scanned in 0xFFFFFFFF. The details of the first 8 errors have been provided. The utility will now report only the count of failed tests. Scan tests: 2, skipped: 0, failed: 1 Do a test using 0xFE03E0E2. Scan tests: 3, skipped: 0, failed: 2 Do a test using 0x01FC1F1D. Scan tests: 4, skipped: 0, failed: 3 Do a test using 0x5533CCAA. Scan tests: 5, skipped: 0, failed: 4 Do a test using 0xAACC3355. Scan tests: 6, skipped: 0, failed: 5 Some of the values were corrupted - 77.3 percent. The JTAG IR Integrity scan-test has failed. -----[Perform the Integrity scan-test on the JTAG DR]------------------------ This test will use blocks of 64 32-bit words. This test will be applied just once. Do a test using 0xFFFFFFFF. Scan tests: 1, skipped: 0, failed: 0 Do a test using 0x00000000. Test 2 Word 0: scanned out 0x00000000 and scanned in 0xFFFFFFFF. Test 2 Word 1: scanned out 0x00000000 and scanned in 0xFFFFFFFF. Test 2 Word 2: scanned out 0x00000000 and scanned in 0xFFFFFFFF. Test 2 Word 3: scanned out 0x00000000 and scanned in 0xFFFFFFFF. Test 2 Word 4: scanned out 0x00000000 and scanned in 0xFFFFFFFF. Test 2 Word 5: scanned out 0x00000000 and scanned in 0xFFFFFFFF. Test 2 Word 6: scanned out 0x00000000 and scanned in 0xFFFFFFFF. Test 2 Word 7: scanned out 0x00000000 and scanned in 0xFFFFFFFF. The details of the first 8 errors have been provided. The utility will now report only the count of failed tests. Scan tests: 2, skipped: 0, failed: 1 Do a test using 0xFE03E0E2. Scan tests: 3, skipped: 0, failed: 2 Do a test using 0x01FC1F1D. Scan tests: 4, skipped: 0, failed: 3 Do a test using 0x5533CCAA. Scan tests: 5, skipped: 0, failed: 4 Do a test using 0xAACC3355. Scan tests: 6, skipped: 0, failed: 5 Some of the values were corrupted - 80.7 percent. The JTAG DR Integrity scan-test has failed.

    Thanks,
    Soumitri

  • Scan integrity test is failing which means there is some issue with hardware. Please do signal integrity check for JTAG signals and make sure it's passing.