Part Number: TMS320F28388D
Hello Team,
Hope you are doing well.
I am currently working on TMS320F28388DPTPSR and using XDS110 Debug Probe for programming the microcontroller.
I am facing the issue of debugger resets when I connect a DMM probe to GND. The issue is coming after programmming the controller & while running the board.
The Hardware connections are :
Pin 1 - TMS : 10K Pull-up to 3V3
Pin 2 - TRSTn : 10K Pull-down
Pin 3 - TDI : TDI of controller
Pin 5 - VTREF : 10K Pull-up to 3V3
Pin 7 - TDO : TDO of controller
Pin 11 - TCK : Pull-up to 3V3
Pin 8, Pin 10, Pin12 : Ground
Pin 4, Pin 6, Pin 9, Pin 13, Pin 14 : Not Conneted
The error is as follows: on CCS
C28xx_CPU1: Error: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 20.0.0.3178)
C28xx_CPU1: Trouble Halting Target CPU: (Error -1135 @ 0x8BB52) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 20.0.0.3178)
C28xx_CPU1: Unable to determine target status after 20 attempts
C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging.
Suggest me wheather is it a issue of Hardware or Firmware? How to solve this?